The Covid-19 pandemic has made it abundantly clear that to overcome the challenges of rising delivery expectations, growing labor shortages and expanding order volumes, the packaging industry will need to embrace automation at a rapid pace. Collaborative robots (cobots) are now increasingly a part of that solution, a trend reflected in the rise of cobot leader Universal Robots that saw a remarkable 75% growth in revenue year-over-year in its most recent global quarterly result.
After a two-year hiatus, PACK EXPO 2021 in Las Vegas, September 23-26, will be the packaging industry’s first in-person opportunity to experience Universal Robots’ longest-reach cobot, the UR10e, featuring a new total payload of 12.5kg (27.55lbs), showcased in Universal Robots’ PACK EXPO booth C3545.
“That’s a 25% increase in payload and a 0% increase in the price of the cobot, giving a significant boost to palletizing applications at no additional expense,” says Joe Campbell, senior manager of applications development at Universal Robots. “That means you can move more per pick, use heavier tools, and process heavier parts, supported by the 1300mm reach (51in) and small footprint that makes the UR10e our best-seller.”
The enhanced UR10e’s greater payload also takes more weight from the hands and shoulders of humans, leading to improved ergonomics and working conditions. With overexertion and repetitive motion accounting for an estimated 24% and 8% of workplace injuries respectively in the U.S. alone, this provides significant relief to human workers.