Universal Robots Debuts the World’s First Cobot Spot Welder and New Palletizing and Machine Tending Cells at Automate

Universal Robots Debuts the World’s First Cobot Spot Welder and New Palletizing and Machine Tending Cells at Automate
Universal Robots Debuts the World’s First Cobot Spot Welder and New Palletizing and Machine Tending Cells at Automate

The cobot pioneer will also celebrate its second representative to receive the Engelberger Robotics Award, the ‘Nobel Prize of Robotics,’ as Global Technical Compliance Officer Roberta Nelson Shea joins the company’s co-founder for this prestigious recognition

Novi, MI, May 11, 2023: Universal Robots (UR) is not only the most widely used collaborative robot arm in the manufacturing industry, the UR cobots have also become the platform of choice for a fast-growing ecosystem of innovative OEM solutions. Nowhere is that more apparent than this year’s Automate, where 60+ UR cobots will be exhibited in more than 30 booths at the show, taking place in Detroit, MI, May 22-25, 2023.

UR’s Automate booth #3623 showcases the latest innovation in a rapidly expanding application field, including the world’s first cobot spot welder, designed and manufactured by Pro Spot International. While other welding technologies such as MIG welding have become popular choices for collaborative robots, spot welding has up until now been prohibitive for cobots due to the weight of the weld gun and the complexity of the welds. With the new i5s resistance spot welder, Pro Spot has developed a lightweight solution, delivering 2-3x more manufacturing capacity than manual spot welding.

“We married our most sophisticated spot welder with Universal Robots’ safe, unrivaled technology,” says Ron Olsson, president and founder of Pro Spot. “The combined platform is a powerhouse of productivity and throughput greatly benefiting any manufacturer who joins sheet metal through spot welding.”

Pro Spot's new i5s resistance spot welder powered by a UR cobot

Another manual welding tool now incorporated in a cobot application is the new rotational positioner from THG Automation, addressing any welder who ever struggled to weld circular or odd-shaped parts.

“Welders use positioners manually all the time, and it was a natural progression for us to incorporate positioners into our collaborative welding system to allow the weldments to be presented to the robot at a more optimal orientation,” says Matt Hendey, CEO of THG Automation, who will be showing the positioner incorporated in his company’s Fronius Perfect Welding CMT system powered by the UR10e cobot.

thg’s cobot weld systems can control up to four rotational positioners, with linear versions coming soon. the positioners are compatible with any ur eseries cobots, so other ur cobot weld systems can use them as well.

Both welding partners—along with many other UR integrators, OEM partners, distributors, and customers—are eagerly looking to incorporate the new UR20 cobot into their applications for added reach and payload capabilities. The award-winning UR20 with 20kg payload and 1750 mm reach starts shipping later this summer and will be showcased at the UR booth in a machine tending application, loading and unloading heavy workpieces into a machine fixture.

The new UR20 cobot can reach further into machines, tend several machines in the same cycle, and handle 25% heavier part* *s. At the show, the cobot is equipped with SCHUNK’s UR+ certified EGP grippers with the ability to handle varying part dimensions

New takes on palletizing and case pack
Manufacturers looking to verify whether a UR cobot palletizer will work for their application can now receive a complete project analysis with performance and installation data, delivered on-the-spot in UR’s booth. With MyRobot.cloud, Rocketfarm is launching the first digital twin solution developed for palletizing with UR cobots. The solution is sought after by integrators who can now quickly verify customer projects on-site, and is showcased with partner Columbia/Okura’s miniPAL®, a mobile palletizing solution powered by the UR10e cobot arm.

example of rocketfarm’s digital twin showing a palletizing application based on customer input.

The flexible miniPAL, with a total workspace footprint of 11’x13’, can palletize at two pallet locations for optimized productivity. The latest design includes three area safety scanners that detect human presence in the palletizing work envelope. This ensures safe (collaborative mode) operation in the presence of workers, while allowing the miniPAL to operate at maximum rates while individuals are not within the palletizing work zone. A ‘big brother,’ the miniPAL+ featuring the UR20 cobot, will be available for preorders in the booth.

Driven by a shared vision of helping manufacturers deploy cobots at scale, Rapid Robotics’ strategic partnership with Universal Robots has supported the company’s expanded offerings to include vital end-of-line applications such as box-building, packing, and palletizing. At the UR booth, Rapid will be displaying a case-packing operation using a UR5e that is integrated with Rapid’s software stack. Attendees can see the pre-trained cobot pick up multiple bottles at once and then pack them neatly into a case, an operation the company has implemented for a major distributor of funeral home supplies.

*Rapid Robotics' case-packing demo to be showcased at Automate*

Multi-tasking cobots in gasketing station, process automation cells, and new operator interfaces

The versatile nature of UR cobots’ ability to handle entire process cycles will be demonstrated by INPRO Technologies’ fully integrated gasketing station for instantaneous curing with plasma treating, liquid gasket dispensing, and UV light. The station features a UR cobot arm performing both assembly/disassembly, material handling, and process control tasks, all while serving as the main coordinating ‘PLC.’

*The multi-tasking UR cobot in INPRO Technologies' Automate demo*

RoboRoom from Reliabotics is a new UR-based 48”x50” modular turnkey automation work cell, designed for a variety of automation applications such as surface deburring & finishing, assembly & test, pick & place, dispensing & bonding, and vision inspection. At Automate, RoboRoom is showcased with an inverted UR5e robot performing metal parts deburring using ATI tools and its own proprietary, recycled CO2 surface-cleaning technology.

The RobotRoom automation work cell from Reliabotics

The new Operator Interface from Robot27 allows operators to easily access and run pre-programmed robot programs and functions without touching the UR teach pendant. Machine operators can execute these tasks with just a few clicks and with no possibility of altering any programming.

“Attendees visiting our Automate booth will quickly realize how our ecosystem continues to innovate on our platform,” says Joe Campbell, senior manager of applications development at Universal Robots. “We’re constantly collaborating with partners on addressing new automation frontiers, with Automate being the perfect discovery pad for our rapidly expanding solution portfolio.”

UR’s Roberta Nelson Shea to receive Engelberger Robotics Award
The ecosystem expansion is enabled by the open platform design originally developed by the company’s co-founder and then CTO Esben Østergaard, who received the Engelberger Robotics Award in 2018 for his pioneering role in the cobot industry. He is now joined by Roberta Nelson Shea, UR’s global technical compliance officer since 2016, who at Automate 2023 receives the prestigious award dubbed ‘The Nobel Prize of Robotics’ for her outstanding work over the course of her career in global robotics safety.

*UR's General Technical Compliance Officer, Roberta Nelson Shea*

For over 45 years, she has been one of the central figures in the development of industrial robot safety standards in North America and around the world. As the convenor of the ISO committee, she led the introduction of ISO/TS 15066, which is the first document that defines standardized safety requirements within human-robot collaboration.

Universal Robots

We believe that collaborative robotic technology can be used to benefit all aspects of task-based businesses – no matter what their size.

We believe that the latest collaborative robot technology should be available to all businesses. The nominal investment cost is quickly recovered as our robotic arms have an average payback period of just six months.

LinkedIn
Local Office
  • Universal Robots USA, Inc
  • 27175 Haggerty Road, Suite 160
  • 48377 Novi, MI
Contact us: +1 844-462-6268
Contact us: + 1-844-GO-COBOT