T
- The (generic) type parameter for the interface representing the type of input data entered or selected by
the end user. Relevant types are, e.g. Integer
and Double
.public interface UserInput<T>
Modifier and Type | Method and Description |
---|---|
T |
getValue() |
void |
setValueChangedListener(ValueChangedListener<T> listener)
Set a listener callback to be notified when the end user changes the associated value as well as when a new
installation is loaded or created.
|
T getValue()
CannotAccessDeprecatedUserInput
- if the user input has been deprecated (using the
CustomUserInputConfiguration.deprecateUserInput(UserInput)
) method)void setValueChangedListener(ValueChangedListener<T> listener)
listener
- the listener callbackCopyright © 2024. All rights reserved.