public interface PrepareToStartScrewdriverParameters
This interface provides parameters relevant for generating script code for the Prepare To Start Screwdriver capability
(registered using ScrewdriverCapabilities.registerPrepareToStartScrewdriverCapability(ScriptCodeGenerator)
).
These parameters are passed when PolyScope calls the implementation of the ScriptCodeGenerator.generateScript(ScriptWriter, Object)
method responsible for the generating the script code.
Copyright © 2024. All rights reserved.