public interface URCapProgramNode extends ProgramNode
ProgramNodeContribution
.Modifier and Type | Method and Description |
---|---|
boolean |
canGetAs(Class<?> urCapProgramNodeInterface)
This method returns
true if a subsequent call to getAs(Class) using the same parameter will be
successful. |
<T> T |
getAs(Class<T> urCapProgramNodeInterface)
The URCap program node contribution (i.e.
|
boolean canGetAs(Class<?> urCapProgramNodeInterface)
true
if a subsequent call to getAs(Class)
using the same parameter will be
successful.urCapProgramNodeInterface
- the interface the program node implements, not null
.true
if the program node can be represented as the specified interface. false
otherwise.<T> T getAs(Class<T> urCapProgramNodeInterface)
The URCap program node contribution (i.e. the class implementing ProgramNodeContribution
) can optionally
implement additional interfaces providing access to various information and/or methods.
If such an interface is implemented, the getAs(Class)
method can be used to retrieve the program node as
said interface.
ProgramNodeContribution
(or an extension/implementation thereof) nor
Object
as argument, otherwise an IllegalArgumentException
is thrown.T
- The (generic) type parameter for the interface.urCapProgramNodeInterface
- the interface the program node implements, not null
.ClassCastException
- If the program node does not implement the interface a class cast exception will be thrown.IllegalArgumentException
- If the type parameter is an implementation/extension ofProgramNodeContribution
or Object
.Copyright © 2024. All rights reserved.