Package | Description |
---|---|
com.ur.urcap.api.domain.payload | |
com.ur.urcap.api.domain.value.dynamics | |
com.ur.urcap.api.domain.value.simple |
Modifier and Type | Method and Description |
---|---|
InertiaMatrix |
PayloadContributionModel.createInertiaMatrix(double ixx,
double iyy,
double izz,
double ixy,
double ixz,
double iyz,
MomentOfInertia.Unit unit)
Creates an inertia matrix to be used when adding a payload to the installation in PolyScope using the method
PayloadContributionModel.addPayload(String, String, Mass, Position, InertiaMatrix) , or updating an existing payload using
PayloadContributionModel.updatePayload(String, Mass, Position, InertiaMatrix) . |
Modifier and Type | Method and Description |
---|---|
boolean |
InertiaMatrix.epsilonEquals(InertiaMatrix other,
double epsilon,
MomentOfInertia.Unit unit)
Indicates whether some other
InertiaMatrix object is "approximately equal" to this one. |
double[] |
InertiaMatrix.getComponents(MomentOfInertia.Unit unit)
Provides the six unique components of the inertia matrix, i.e.
|
double |
InertiaMatrix.getIxxComponent(MomentOfInertia.Unit unit)
Provides the Ixx component of the inertia matrix, i.e.
|
double |
InertiaMatrix.getIxyComponent(MomentOfInertia.Unit unit)
Provides the Ixy component of the inertia matrix, i.e.
|
double |
InertiaMatrix.getIxzComponent(MomentOfInertia.Unit unit)
Provides the Ixz component of the inertia matrix, i.e.
|
double |
InertiaMatrix.getIyyComponent(MomentOfInertia.Unit unit)
Provides the Iyy component of the inertia matrix, i.e.
|
double |
InertiaMatrix.getIyzComponent(MomentOfInertia.Unit unit)
Provides the Iyz component of the inertia matrix, i.e.
|
double |
InertiaMatrix.getIzzComponent(MomentOfInertia.Unit unit)
Provides the Izz component of the inertia matrix, i.e.
|
Modifier and Type | Method and Description |
---|---|
static MomentOfInertia.Unit |
MomentOfInertia.Unit.valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static MomentOfInertia.Unit[] |
MomentOfInertia.Unit.values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
Copyright © 2024. All rights reserved.