Articles Download Safety & Security Forum myUR Go to Main Site

Universal Robots A/S
Energivej 51
DK-5260 Odense S

T: +45 8993 8989
sales@universal-robots.com

 
  • Articles
  • Download
  • Safety & Security
  • Forum
  • myUR
  • Go to Main Site
  • Support
  • Articles
  • Actinav - Cable Management tech note

Actinav - Cable Management tech note

Electric Cable Management for ActiNav

Last modified on May 02, 2022

Create Date: January 21st, 2020

Introduction


ActiNav autonomously does all of the robot motion planning for transporting parts from a bin to their destination. Since parts may be anywhere in the bin, in any orientation, each path is different. Typical cable and hose management schemes, which rely on a predictable, contained path, are often insufficient for the wide variety of possible ActiNav movements. Standard cable management schemes are also too bulky and do not have enough flexibility. Cables may become tangled, or may catch on elements in the environment.
This article describes one way of managing electrical cables for bin picking using coiled cables.
See the note at the end about combined pneumatic/electrical systems.

 

Recommended Parts List

Part reccomended sources

Coiled cable

Tensility 31-00xxx (depending on gauge and number of conductors)

Digi-Key, Arrow

Polyethylene tubing

1⁄2” / 12.5 mm inner diameter semi-flexible tubing

McMaster-Carr 50375K51

Deformable PTFE tape

0.0045” (0.11 mm) thick, 2” (51 mm) wide

McMaster-Carr 76025A715

Prerequisites

  • Coiled cable. The number of conductors depends on your end effector.
    • For bridging the last 3 wrist joints and the tightest connection to the robot, we recommend a coiled cable with an outer spiral diameter of 25 mm / 1 inch or less. Tensility (https://tensility.com) makes coiled cables containing three to eleven stranded wires from 18 to 28 AWG that are well suited (part numbers 31-00xxx).
    • It is also possible, but not preferred, to use a coiled USB cable. Most cables are too short:
      be sure you use a minimum 6 ft / 1850 mm extended length. USB cables are not as robust, stretch more, and will wear faster.
  • Semi-flexible polyethylene tubing of a smaller inner diameter than the outer coil diameter of
    the cable. For a 25 mm / 1 inch coil, use 12.5 mm / ½” inner diameter tube. For a 15 mm / 0.6“
    USB coiled cable, use a 9.5 mm / ⅜” inner diameter tube. Exact dimensions are not important:
    what matters is that the cable needs to be wound tighter than its relaxed state to be forced in to
    the tube.
  • Deformable PTFE tape. 0.0045” (0.11 mm) thick is easiest to handle, and seams don’t cause significant catch points. Use narrow tape for the rubber rings and wide tape for friction reduction, or use wide tape for both. https://www.mcmaster.com/76025A715
  • Hose clamps: We recommend stainless steel clamps that are made for soft hose. These are smooth and have upturned edges, and are less likely to mar the robot finish:
  UR5 UR10

Lower joints

https://www.mcmaster.com/5076K53 https://www.mcmaster.com/5076K54

Lower tube

https://www.mcmaster.com/5076K53 https://www.mcmaster.com/5076K53

UR5: Lower joints: https://www.mcmaster.com/5076K53 Lower tube https://www.mcmaster.com/5076K53

UR10: Lower joints: https://www.mcmaster.com/5076K54 Lower tube: https://www.mcmaster.com/5076K53

  • (Optional) PVC tape to protect the robot
  • Tools: A screwdriver for the hose clamps, fine toothed hacksaw or tube cutter, pointed (X-Acto)
    knife, scissors.

 

Determine your configuration

For ActiNav bin picking, the three wrist joints tend to have the greatest range of movements, and thus need the most flexibility in cable management. It is generally sufficient to use the coiled cable just to bridge these last three joints. You can transition back to regular cable with service loops for the base, shoulder, and elbow joints.

Prepare the cable

The coiled cable needs to be held close to the robot in a way that keeps it in place, but doesn’t create wear points or pinch points that will cause the cable to fail. The best way to do this is to attach it with the semi-flexible polyethylene tubing. Never clamp a cable directly to the robot: this will fail in just a few days.

  1. Cut a piece of polyethylene tubing about 25 mm / 1 inch long. Use a fine-toothed saw or a tube cutter: if you can cut it with a knife, the tubing is too flexible.
  2. Sand the edges of the tubing to remove cut marks.
  3. Round off the inside corners of the tubing with the pointed knife.
  4. Push the cable through the pieces of tubing. Generally, you can just pull it through. Depending on your end effector, there should be about 16 loops between one tube and the end; and about 14 loops between the two tubes for the UR5, and about 19 for the UR10.
  5. Twist the coiled cable more tightly to pack it inside of the polyethylene tube. Ensure the right number of coils next to the tubes are still present as specified in step 4.

 

Prepare the robot

Tape the joints: The cable may rub against the rubber flat-rings that seal the robot joints, damaging the rubber. Also, the cable will abrade against the rough joint castings. At minimum, protect the flat-rings with a layer of PTFE tape. Note in the picture which side of the joint to place the tape on, so that the joint isn’t bridged by the tape. (A pneumatic end effector is shown, but the same principle applies). Do not use PVC tape. PVC deforms when the joint heats up and may “creep”.

Determine where to route the spiral tubing: Determine what the most likely robot pose is for picking and placing, and route the cable so it is least likely to interfere with the bin, placement target, or environment. This is generally best achieved by routing the tube over the top of the robot when it is positioned over the bin (see left top picture, below). You may want to run your ActiNav bin picking program first, to observe typical movements.

For difficult picks, especially when free spin around the tool Z axis is enabled, the robot may assume a wide variety of poses. Be sure that, whatever routing you choose, there is enough room for any wrist joint to rotate at least ±180°.

Use of coiled cabling is no guarantee that the cable will not interfere with the bin, environment, or placement. The amount of slack required for full joint rotations may protrude or sag.

Clamp down the tubes: Using the right size hose clamp, clamp one tube to wrist joint 2, near the connection with wrist joint 1. Clamp the other to the lower robot tube, near wrist joint 1. You may optionally use PVC tape under the clamps to protect the robot from scratches. When clamping, slightly crush (deform) the tube, to lock the coiled cable in place.  

Hose clamps and worm drives may have sharp edges. Account for this in your risk assessment! Also, locate the worm drive screws so they are unlikely to contact the cable. Occasional contact is generally OK.

Tape the wrist joints against abrasion: It is preferable to also reduce the friction of the cable rubbing across the robot joint.

Exercise the three wrist joints through at least ±240° (simultaneously, not just individually). Observe the places where the cable slides over the castings. Use the PTFE tape to cover the joints to minimize abrasion. It’s not required to cover every last spot, just the major rub points and the rubber rings.

WEAR and replacement

The cable may stretch or abrade over time. Properly routed, stretch will be minimal. USB cables will stretch more over time (see picture at right). Keep this in mind when routing the cable, and replace it if it gets too long or too worn. When replacing the cable, it’s a good idea to replace or supplement the PTFE tape also.

Typical Lifetime
Without friction reduction, ignoring stretch

  • Heavy duty cable: 23 weeks
  • USB cable: 12 weeks

With friction reduction, ignoring stretch

  • Heavy duty cable: > 2 years

  • USB cable: 1 year

Wear mechanisms

Without friction reduction:

  • Abrasion wears off the cable jacket, eventually exposing the wiring inside. This may short against the robot body or against another wire. Abrasion may be visible by the formation of dust, or just by inspecting the cable.

With friction reduction

  • Eventually, the internal wires will break at a stress point. This will cause intermittent connections at stressed cable positions. USB cables are generally more fragile, and will develop micro-breaks along the entire length (see green wire in picture). This will cause frequent intermittents.

 

Combined pneumatical and electrical connections

For end effectors that require both pneumatic and electrical connections, it is possible to route the electrical cable inside of the coiled pneumatic tube.

In cases like this, the pneumatic tube should be attached according to the instructions in https://www.universal-robots.com/articles/ur/actinav-pneumatic-hose-management/ and the electrical cable can simply ride inside of the pneumatic tube. Be sure to anchor the electrical cable at both ends, so that the cable and the tube each are responsible for maintaining the same amount of tension as the robot moves, i.e. you shouldn’t make the tube carry the cable weight.

Never clamp a cable directly to the robot. This will fail in a few days.

 

Related articles

ActiNav - Adding a safety laser scanner to a work station
Actinav: Pneumatic Hose Management
Actinav - Creating your own part models with the Einscan SE
ActiNav - Creating a Simplified Part Model using Solidworks
Actinav - Cable Management tech note
ActiNav - Re-grip logic and Sample Progam
End User Software License Agreement (EULA) - ActiNav
Updating ActiNav to the latest version
ActiNav - Integrating a signal light
ActiNav Clearance Shapes Creation and Use
ActiNav v1.3.0 Release
ActiNav Autonomous Bin Picking
Palletizing with ActiNav
Sample ActiNav Program
ActiNav Adding safety laser scanner to ActiNav work cell
ActiNav Remote access - Ixon
ActiNav Rescan - Sample Program
logo

Product

  • UR3e Robot
  • UR5e Robot
  • UR10e Robot
  • UR16e Robot
  • UR20 Robot
  • UR+ Products

Company

  • About us
  • Contact us
  • Careers We're hiring
  • UR merchandise

Training / Resources

  • Academy
  • Technical Resources
  • Articles
  • FAQ

Insights

  • Blog
  • Case stories
  • Content library
  • News centre
  • Podcast
  • Webinars & Events

Get in touch

  • Ask an Expert
  • Schedule a no-cost assessment
  • Find a distributor
  • Customer support

Connect with us

  • LinkedIn
  • Facebook
  • Twitter
  • YouTube
  • Instagram
  • Universal Robots A/S
  • Energivej 51
  • DK-5260 Odense S
  • T: +45 89 93 89 89
  • sales@universal-robots.com
  • US Corporate Office
  • 27-43 Wormwood St.
  • 02210 Boston, MA.
  • +1-844-GO-COBOT
  • ur.na@universal-robots.com
  • Copyright @ Universal Robots 2026
  • Cookie policy
  • Privacy policy
  • Universal Robots A/S
  • Energivej 51
  • DK-5260 Odense S
  • T: +45 89 93 89 89
  • sales@universal-robots.com
  • US Corporate Office
  • 27-43 Wormwood St.
  • 02210 Boston, MA.
  • +1-844-GO-COBOT
  • ur.na@universal-robots.com

Copyright © Universal Robots 2026

Cookie policy
Privacy policy