Articles Download Safety & Security Forum myUR Go to Main Site

Universal Robots A/S
Energivej 51
DK-5260 Odense S

T: +45 8993 8989
sales@universal-robots.com

 
  • Articles
  • Download
  • Safety & Security
  • Forum
  • myUR
  • Go to Main Site
  • Support
  • Articles
  • Connecting to Client Interfaces within URSim

Connecting to Client Interfaces within URSim

This is a guide to connect to the Client Interfaces within URSim

Last modified on Sep 11, 2025

ACCESSING CLIENT INTERFACES ON URSIM

Network Setup within the URSim interface does not currently allow users to set a static IP address. In order to test that an application correctly communicates within URSim, follow the procedure below to gain access to the client interfaces.

  1. Set Network to Dynamic Host Configuration Protocol (DHCP)

Within your Virtual Machine of choice, open URSim and navigate to Setup Robot > Network . Select the first checkbox, DHCP. Note that selecting “Static Address” will allow you to enter an IP Address and gateway, but will not actually configure URSim to your selected address.

  1. Read your actual IP Address

Within the virtual machine open a terminal. Type in “ifconfig” and note the IP address of eth0. This will be the IP address of the robot within URSim.

 

  1. Match the Client Machine IP Address

Configure the PC or device or choice to have a matching IP address. In the example image above, a matching IP address to 192.168.238.128 would be 192.168.238.22. Note that the first three digits are matching, and the last is different. For a Windows System running a Virtual Machine, go to Network, click Change Adapter Settings, and open the properties for Network Adapter. Configure the Static IP address for IPv4.

 

  1. Test Server Functionality

Utilize a communication utility such as SocketTest to verify a connection can be made with URSim. In order to test the “running” command using the Dashboard server, use the IP address of URSim from Step 2, and use 29999 for the port. Provide the “running” command and verify the correct response.

logo

Product

  • UR3e Robot
  • UR5e Robot
  • UR10e Robot
  • UR16e Robot
  • UR20 Robot
  • UR+ Products

Company

  • About us
  • Contact us
  • Careers We're hiring
  • UR merchandise

Training / Resources

  • Academy
  • Technical Resources
  • Articles
  • FAQ

Insights

  • Blog
  • Case stories
  • Content library
  • News centre
  • Podcast
  • Webinars & Events

Get in touch

  • Ask an Expert
  • Schedule a no-cost assessment
  • Find a distributor
  • Customer support

Connect with us

  • LinkedIn
  • Facebook
  • Twitter
  • YouTube
  • Instagram
  • Universal Robots A/S
  • Energivej 51
  • DK-5260 Odense S
  • T: +45 89 93 89 89
  • sales@universal-robots.com
  • US Corporate Office
  • 27-43 Wormwood St.
  • 02210 Boston, MA.
  • +1-844-GO-COBOT
  • ur.na@universal-robots.com
  • Copyright @ Universal Robots 2025
  • Cookie policy
  • Privacy policy
  • Universal Robots A/S
  • Energivej 51
  • DK-5260 Odense S
  • T: +45 89 93 89 89
  • sales@universal-robots.com
  • US Corporate Office
  • 27-43 Wormwood St.
  • 02210 Boston, MA.
  • +1-844-GO-COBOT
  • ur.na@universal-robots.com

Copyright © Universal Robots 2025

Cookie policy
Privacy policy