Complex pattern pallet example
Complex pattern pallet example, palletizing in a (more) complex pattern.
Examples are valid for:
CB2 Software version: 1.8.16941
CB3 Software version: 3.1.17779
e-Series Software version: All versions
Note that older or newer software versions could behave different.
These examples can be used for both CB2, CB3 and e-Series.
One example of make pallet with two separate small pallet pattern.
This example show how to do more than one more pallet in one surface, you will need to initialize the different pallet pattern parameters including step distance and counts in X and Y direction. After two pallet have been done in one layer, the Z direction will add once and do the repeat cycle again.
This sample program can also be used to do more complicated cases like you will do external treatment for some particular pallet number and just need to add simple if statement in program.