Articles Download Safety & Security Forum myUR Go to Main Site

Universal Robots A/S
Energivej 51
DK-5260 Odense S

T: +45 8993 8989
sales@universal-robots.com

 
  • Articles
  • Download
  • Safety & Security
  • Forum
  • myUR
  • Go to Main Site
  • Support
  • Articles
  • Creating a cycle timer via Polyscope

Creating a cycle timer via Polyscope

Last modified on Jun 20, 2016

An example of how to create a cycle timer via polyscope.

Examples are valid for:
CB2 Software version: 1.8.16941
CB3 Software version: 3.3 and under
Note that older or newer software versions may behave differently.

These examples can be used for both CB2 and for CB3.

 

This programming technique will allow you to create an accurate cycle time for any program, see screen shot below:

 Capture

 

The variable ‘timer’ in the BeforeStart is just to initialize the timer at time zero, it is then referenced again in the thread where it starts from 8ms (milliseconds) and will count until the program is haulted.

The 8ms (.008) is added to the timer because that is the cycle time for the proccesor of the robot so by adding this time it gives the presise time it took the program to run without effects of the robots OS.

The ‘MoveJ’ consists of three arbitrary waypoints to show a cycle time for this example, customers program would replace that portion, inside the rectangular box.

To get a single cycle time, the program should end with a ‘Halt’ or the check box for “Program loops forever” should be unchecked so that the timer displays one cycle time instead of continually running. 

logo

Product

  • UR3e Robot
  • UR5e Robot
  • UR10e Robot
  • UR16e Robot
  • UR20 Robot
  • UR+ Products

Company

  • About us
  • Contact us
  • Careers We're hiring
  • UR merchandise

Training / Resources

  • Academy
  • Technical Resources
  • Articles
  • FAQ

Insights

  • Blog
  • Content library
  • News centre
  • Podcast
  • Webinars & Events

Get in touch

  • Ask an Expert
  • Schedule a no-cost assessment
  • Find a distributor
  • Customer support

Connect with us

  • LinkedIn
  • Facebook
  • Twitter
  • YouTube
  • Instagram
  • Universal Robots A/S
  • Energivej 51
  • DK-5260 Odense S
  • T: +45 89 93 89 89
  • sales@universal-robots.com
  • US Corporate Office
  • 27-43 Wormwood St.
  • 02210 Boston, MA.
  • +1-844-GO-COBOT
  • ur.na@universal-robots.com
  • Copyright @ Universal Robots 2026
  • Cookie policy
  • Privacy policy
  • Universal Robots A/S
  • Energivej 51
  • DK-5260 Odense S
  • T: +45 89 93 89 89
  • sales@universal-robots.com
  • US Corporate Office
  • 27-43 Wormwood St.
  • 02210 Boston, MA.
  • +1-844-GO-COBOT
  • ur.na@universal-robots.com

Copyright © Universal Robots 2026

Cookie policy
Privacy policy