UR Log Viewer - Release Notes
Release Notes for the UR Log Viewer
Created: October 16th, 2023
Download the UR Log Viewer HERE
RELEASE NOTES FOR UR LOG VIEWER VERSION 1.3.5.0
NEW FUNCTIONALITY
- UR30 support
RELEASE NOTES FOR UR LOG VIEWER VERSION 1.3.4.0
NEW FUNCTIONALITY
- Bug fix on RTDE Elbow values.
RELEASE NOTES FOR UR LOG VIEWER VERSION 1.3.3.0
NEW FUNCTIONALITY
- Bug fix on data visualization for UR10e 12.5kg
RELEASE NOTES FOR UR LOG VIEWER VERSION 1.3.2.0
NEW FUNCTIONALITY
- Torque Chart
- Speed Scaling in velocity charts visible
- Record value selection changed
- Live View removed
- Record default values aligned to ur_service file
- Error codes updated
- UR20 support
- Polyscope 6 support
Release Notes for UR Log Viewer version 1.2.1.0
Release date: May 20th, 2021.
New functionality
- Real-time data graphs
- Y Axis in all charts zoom able
- new chart for Payload/CoG
- new chart Inertia
- new chart FTSensor
- Tool tip errort-imeline legend(error description)
- Text search result now depending on filter check boxes
- Default recording values changed: Checkboxes, time (5min max) and frequency (500)
Bugs
- Wrong Current window (LA-41)
- Better catching damaged files
- flightrecords
- zip files
- logfiles
- Text search field reset if you delete all character
- Error Timeline remove double entries
Release Notes for UR Log Viewer version 1.2.0.0
Release date: January 13th, 2020.
New functionality
- Real-time data graphs
- Force Chart, Joint Temperature Chart, Joint Voltage Chart, GP IO Chart.
- Improved general design of all charts.
- RTDE Values GP INT and GP Float implemented.
- Log Reader
- Log data will be reloaded if language is changed.
- Added option to "Open all Groups" in Log Reader Tab.
- Option for an aggregate view in Error Timeline.
- Improved performance, including when loading larger sets of data
- MSI installation type.
Release Notes for UR Log Viewer version 1.1.0.0
New functionality
- Real-time data graphs
- In real-time data view, the script line number is shown on the Position graph.
This enables easily to correlate real-time data with the relevant sections of the executed user program. - This is only available with robots w. PolyScope 5.9/3.14 and above. If a lower version is used where script line is not recorded, the index is shown.
- In real-time data view, the script line number is shown on the Position graph.
-
Log History overview
-
It is now possible to copy multiple lines of log messages
Multiple lines can be selected while holding CTRL or SHIFT - Focus is kept on the selected error code, if view is changed (selecting Info, Warning, etc.)
-
- New error code timeline view
- A new view of a timeline of error occurrence over time can be shown by right-clicking selected error codes in the Log History view.
- Users are able to select default error codes, or show only selected errors
- Users are able to toggle between bar and graph charts
- Users can select desired start-and end-dates for the timeline view
- Log Analysis
- If CB3 Polyscope version is older than 3.12, the version field is marked red and a message will be displayed.
- Data Recording
- Simplification of the RTDE values to record
- Implemented tool-tips to describe RTDE fields
- Ability to perform continuous recordings.
This enables to record data over longer periods of time, eg. to track less-frequently occurring issues- Users can select the amount of time recorded per file
- Log Viewer will create a new recording file for each increment of the selected recording time until recording is stopped
- We recommend to configure 100Hz and 30min settings for longer periods.
- Language support
- Users can now select language in the Help-tab
- Implemented the following user interface and error code description languages:
EN DE DK FR ES PT RU ZH TR - The following languages are only available for error codes (with EN user interface).
IT NL JP CS KO HU PL NO RO SK SL SV - Developer Messages are not translated.
Bug fixes
- Fixed an issue where the backup log history (with .bak-extension) was not exported in "Export from robot"-tab
- Fixed an issue where clicks caused wrong actions
- General performance improvements