Good Practice for Long-term Storage
Good practice for long-term storage of robots and spare parts
This article describes some general guidelines for long-term storage of robots and spare parts. This Applies for all robot generations.
A robot is considered long-term stored when it is stored for a period of 6 months or more.
In order to keep the robot and spare parts in its best possible condition, it is recommended to follow normal good practice which is:
- Storage temperature: 10-30°C
- Humidity: RH20-60%
- Universal Robots recommends to unpack and startup robot at least yearly and let them run a light load program rotating in all joints at least 90degree 5 times in each direction to distribute the lubricants. If possible, also mount spare parts joints on an arm and do the same operation routine.
- In rare occurrences there might be a need for wiping down the robots after storage to remove any excess lubricants that have migrated out of the sealings.
- The battery is designed to last for the lifetime of the robot and will not be charged when power is applied to the system. The battery service life is 8 to 10 years but can for e-Series and UR20/UR30 be replaced.
- Flash memory can lose their data capacity over time, therefore there is a potential risk that the data on e.g. the SD-card will have to re-flashed. See New Image Installation.