Power Supply Unit (PSU) for AC to DC for testing OEM DC Controller
Clarification of PSU choice for AC to DC for testing an OEM Controller
Recap of Electrical specifications for the OEM Control Box. Same information can be found in the OEM Control Box Installation Guide (section 8. OEM Control Box Specifications)
AC Variant
Property | Min | Typical | Max | Unit |
Input Voltage | 90 | 100 - 240 | 264 | VAC |
External Mains Fuse (@ 90-200V) | 15 | - | 16 | A |
External Mains Fuse (@ 200 - 265V) | 8 | - | 16 | A |
Input Frequency | 47 | - | 440 | Hz |
Stand-by Power | - | - | <1.5 | W |
DC Variant
Property | Min | Typical | Max | Unit |
Input Voltage | 19 | 24 - 48 | 72 | VDC |
Stand-by Power | - | - | <7 | W |
External fuse | - | - | 100 | A |
Inrush current (200) | - | - | 400 | A |
It is Universal Robots recommendation that if one insists of using an AC/DC to DC/DC setup, to use our own LCM1500W-T 48V PSU, P/N: 177526. This is the same PSU that is used for UR5e/UR10e/UR16e.
If one chooses not to use the recommended PSU, it should be noted that Universal Robots takes no responsibility.
Furthermore, one should not run a program that requires more power than a certain PSU can deliver. If unsure of how much power is needed, modify the configuration file. This is done in a terminal by typing nano .urcontrol/urcontrol.conf. In the subsection [Hardware] change to power_supply = 750 when a 36V or 48V battery supply is used. When a 24V battery supply is used, change to power_supply = 500
In case an UR3e is used, then power_supply = 600 when a 36V or above battery supply is used.