Serial numbers
Understanding Universal Robots serial numbers
General SN:
UR20 / UR30 SN:
OEM vs. Standard Robots:
(Only applicable for e-series)
How to differentiate standard robots from OEMs is from the SN structure:
SN structure: YYYY (year) G (generation) S (size) XXXXX (production number).
The number from the OEM starts with:
- 90000 if DC OEM
- Eg.: 20215590001
- 80000 if AC OEM
- Eg.: 20215580001
E-Series
|
Made from |
Made to |
Serial no. from |
Serial no. to |
UR3e |
2018 |
Still in production |
20185300000 |
Still in production |
UR5e |
2018 |
Still in production |
20185500000 |
Still in production |
UR10e |
2018 |
Still in production |
20185000000 |
Still in production |
UR16e |
2019 |
Still in production |
20195600000 |
Still in production |
The control boxes have changed for both CB3.1 and e-Series in June 2019: https://www.universal-robots.com/articles/ur/documentation/product-alert-control-box-updates-june-2019/
UR10e 12,5Kg vs. 10Kg:
The UR10e - 12,5Kg has a different number than the old UR10e - 10Kg:
- UR10e 10Kg: YYYY (year) 5 (e-Series Generation) 0 (10Kg) 00000 (Production Number)
- Eg.: 20215000001
- UR10e 12,5Kg: YYYY (year) 5 (e-Series Generation) 2 (12,5Kg) 00000 (Production Number)
- Eg.: 20215200001
cb3.1
|
Made from |
Made to |
Serial no. from |
Serial no. to |
UR3 |
2015 |
Still in production |
2015330001 |
Still in production |
UR5 |
2016 |
Still in production |
2016351864 |
Still in production |
UR10 |
2016 |
Still in production |
2016301779 |
Still in production |
UR3
- The CB3.1 controller is a bit different from the CB3.0 controller due to the following
- It runs of a USB version with more process power
- It runs of a USB key (USB 3.0) where all former CB-versions runs of a flashcard
The control boxes have changed for both CB3.1 and e-Series in June 2019: https://www.universal-robots.com/articles/ur/documentation/product-alert-control-box-updates-june-2019/
cb3
|
Made from |
Made to |
Serial no. from |
Serial no. to |
UR5 |
2014 |
Still in production |
2014350001 |
2016351863 |
UR10 |
2014 |
Still in production |
2014300001 |
2016301778 |
CB2 and CB3 looks the same on the outside. However, on the inside there are many differences. Here is a quick overview of the differences.
- True absolute magnetic encoders
- Old type UR uses incremental optical encoders
- Each mark on encoder disk is unique, making it unnecessary for battery backup
- This results in no referencing needed at power up and other advantages
- Safety Control Board (CB3) replaces Masterboard(CB2)
- Additional I/O, Total is now 16 inputs and 16 outputs in control box
- 8 inputs and 8 outputs are easy configurable as Safety signals or general-purpose signals
- Connectors replaces screw terminals
- Connectors are hardcoded, avoids incorrect insertion
- UR Safety 3.0, Patented adjustable Safety System
- UR Safety 3.0 is certified by TÜV
- All safety functions are safety rated to Performance Level d (PLd)
Tested in accordance with:
EN ISO 13849:2008 PLd
EN ISO 10218-1:2011, Clause 5.4.3
- Software improvements
- Program execution will continue from where it stopped (result of the true absolute encoder)
- Realtime performance, part of software re-written
- Conveyor tracking, decoding of encoders now runs at 40kHz (CB2: 125Hz)
- Singularity, speed is reduced around singularities, so the robot is able to move through singularities
cb2
|
Made from |
Made to |
Serial no. from |
Serial no. to |
UR5 |
2011 |
2012 |
1 |
Approx. 934 |
UR5 (Motor Update) |
2012 |
2014 |
Approx. 935 |
2147 |
UR10 |
2012 |
2014 |
1 |
745 |
Photo of a CB2 with controller
(UR10 controller has an additional power supply but the look the same on the outside)
UR5
UR10
The “end of Support” for CB2 is scheduled for the 30/06/2022: https://www.universal-robots.com/articles/ur/documentation/product-alert-end-of-support-cb2/
CB1
|
Made from |
Made to |
Serial no. from |
Serial no. to |
|
UR5 |
2007 |
2011 |
1 |
217 |
|
Note: The controller on a CB1 can be updated to a CB2. Ask Global. Prod. Supp. about price and how |
|
Photo of a CB1 robot and the controller
UR5 (CB1, UR5’s is also called UR-6-85-5-A)