Product Alert: Safety Notice PROFIsafe
Universal Robots A/S expressly disclaims liability for any and all damages or injuries caused as a result of customer’s failure to install, operate and maintain the robot in strict compliance with the User and Service Manuals, train personnel as needed for the application, follow and implement the recommendations in this safety notice.
![]() ![]() |
Universal Robots expressly disclaims liability for any and all damages or injuries caused as a result of customer’s failure to install, operate and maintain the robot in strict compliance with the User Manual and Service Manual, train personnel as needed for the application, follow and implement the recommendations in this safety notice. |
Official Safety Notice(s) on the bottom of the page
To: Universal Robots Customers of PROFIsafe
From: Universal Robots Global Technical Compliance
Date: 15 October 2024
Subject: SAFETY NOTICE PROFIsafe
www.universal-robots.com/articles/ur/safety/safety-notice-profisafe/
During our on-going quality assurance efforts, a minor issue was discovered relating to the use of:
- PROFIsafe combined with an external 3-Position Enabling Device
- PROFIsafe combined with a 3-Position Enabling Teach Pendant (3PE TP).
The issue can inadvertently lead the operator to believe there is no program running even if the robot is in fact being controlled by a program.
The issue does not compromise any of the safety features of our robots. However, it is possible that an operator can be confused about the control of a robot.
This confusion can lead to hazardous situations.
The software versions affected when an external 3PE device, or a 3PE TP, is used are as follows:
- SW 5.13
- SW 5.14
- SW 5.15
- SW 5.16
- SW 5.17
- SW 5.18
SW 5.12 LTS is not affected
|
WARNINGInjury can result from use of UR robots using PROFIsafe combined with an external 3PE device, or using PROFIsafe combined with a 3PE Teach Pendant and SW 5.13 to 5.18. To prevent this hazardous situation, upgrade the SW to version 5.18.1 or higher. |
If you have any questions about this Safety Notice, please email questions to SafetyNotices@Universal-Robots.com and these will be directed to your regional representative. You may locate and contact your regional Universal Robots representative directly at https://www.universal-robots.com/about-universal-robots/contact-info/.