Safety FAQ
This section contains questions and answers on different safety topics related to the installation and use of UR robots.
A comprehensive summary about robot safety is available: Safety Made Easy
For better understanding our TÜV certificates, a document called Safety description and functional safety details has been made to explain the different safety functions, what they involve and what is controlled when the function is activated. Please find the document from the download section.
CB3 safety description and functional safety details
e-Series safety description and functional safety details
See bottom off page for download in Chinese
Topic: Definitions
Question |
Answer |
What is a “Stop Category”? |
“Stop Category” is a classification of how robot motion is stopped in a safe way. There are three different types. |
What is ”Cat 3” or |
The term “Category” should not be confused with the term “Stop Category”. “Category” refers to the type of architecture used as basis for a certain “Performance Level”. A significant property of a “Category 3” architecture is that a single fault cannot lead to loss of the safety function. (See ISO 13849-1 for more details) |
What is ”PLd” or |
A Performance Level (PL) is a discrete level used to specify the ability of safety-related parts of control systems to perform a safety functions under foreseeable conditions. PL=d is the second highest reliability classification, meaning that the safety function is extremely reliable. (See ISO 13849-1 for more details) |
What is SIL 2? |
SIL (Security Integrity Level), like Performance level, is a measure of how likely it is that a dangerous failure will occur in a system. SIL 2 roughly equivalent to PL d (performance level d). |
Topic: Risk Assessment
Question |
Answer |
What is a risk assessment? |
A risk assessment is the overall process of identifying all risks and judging if they are reduced to an appropriate level. It includes both risk analysis and risk evaluation. |
What is a risk analysis? |
A risk analysis is a combination of the specification of the limits of the robot installation, hazard identification and risk estimation. |
What is a risk estimation? |
Risk estimation is defining likely severity of harm and probability of its occurrence. |
What is a risk evaluation? |
A risk evaluation is the judgment, on the basis of risk analysis, of whether the risk reduction objectives have been achieved. |
What is a residual risk? |
A residual risk is the risk remaining after protective measures have been implemented. |
Topic: Standards
Question |
Answer |
Is it required for robots to comply with ISO 10218-1? |
It is required to comply with the laws and regulations in the country and/or the state that the robot is installed. Some countries require that robots comply with ISO 10218-1 or the equivalent national standard. ISO 10218-1 (robot) & ISO 10218-2 (integration) have been adopted in Europe, USA (ANSI RIA R15.06), Canada (CA Z434), and various countries by reference (Brasil, Japan, Korea, China). |
Do UR robots comply with |
Yes – CB3 and e-Series robots have 3rd party certification to EN ISO 10218-1, which is identical to ISO 10218-1. A Technical Specification with clarifications on the features described in ISO 10218-1 is published in February 15th 2016 under the name ISO/TS 15066. |
Are UR robots designed for collaborative operation according to ISO 10218-1? |
UR Robots comply with the requirements for collaborative operation defined in ISO 10218-1:2011, clause 5.10.5. (Power and Force Limiting). A risk assessment of the complete robot application is required. |
What is the difference between ISO 10218-1 and ISO 10218-2? |
- ISO 10218-1 is for robots. UR is the manufacturer of robots, which are required to comply with ISO 10218-1. A "naked" robot without an end-effector is considered partly completed machinery. As a result, robots are not allowed to be CE-marked. |
What is ISO/TS 15066, Technical Specification on Collaborative Robots? |
ISO/TS 15066 is NOT a standard, but a Technical Specification with additional guidance for collaborative robot applications published February 2016. It contains guidance on risk assessment for the integration of robots in collaborative applications. It also includes an informative annex with a research study on biomechanical thresholds. |
What is ISO 13849? |
These standards defines how a safety-related control system must be designed and implemented to achieve a specific performance level. |
What is IEC 62061? |
IEC 62061 is roughly equivalent to ISO 13849-1. The two standards defines safety-performance-levels using the same principles, but are developed by two different international committees. SIL levels from IEC 62061 can be directly translated to Performance Levels in ISO 13849-1 and vice versa. |
Topic: UR Robots Safety
Question |
Answer |
What is a Stop Category? |
“Stop Category” is a classification of stopping. There are three different types: |
Which Stop Category is used for emergency stop in UR robots? |
The UR robots emergency stop is designed as a Stop Category 1 stop. |
Which Stop Category is used for safeguard stop in UR robots? |
The UR robots safeguard stop is a Stop Category 2 stop. In ISO 10218-1 and ISO 10218-2, the safeguard stop is called a “protective stop”. In comparison, UR robots use the term “protective stop” for non-safety related robot stops |
What is the difference between emergency stop and safeguard stop? |
- Emergency stop functions are to be used for emergencies only. An emergency stop is manually actuated by a person pressing the red emergency pushbutton that has a yellow background in accordance with ISO 13850. Use of the emergency stop should be for emergencies and therefore be infrequent and not part of a daily routine. |
What is the Machinery Directive 2006/42/EC? |
The European Machinery Directive (MD) is one of many Directives forming laws in the European Union (EU), and its official number is "2006/42/EC". Some countries outside EU also implements these Directives.
http://eur-lex.europa.eu/legal-content/EN/TXT/?qid=1426848262724&uri=CELEX:32006L0042 NOTE: Typically it is easy to find Directives by searching the number on Google.com (E.g. "2006/42/EC" ). Also see the "Declaration of Incorporation" in the UR user manual. |