<link rel="stylesheet" href="styles-ENMP3CLZ.css"> Skip to main content

Lightweight Cobots Take on Heavy-duty Jobs — Even Welding

Sure, cobots are lightweight: the largest UR10 robot is under 29 kg/64 lbs, so they’re easy to pick up and move from one process to another. But they’re no lightweights when it comes to heavy-duty processes like welding. In fact, there’s already a range of cobot welding systems to choose from. Surprised? Don’t be. It’s just...

Lightweight Cobots Take on Heavy-duty Jobs — Even Welding
Lightweight Cobots Take on Heavy-duty Jobs — Even Welding

Sure, cobots are lightweight: the largest UR10 robot is under 29 kg/64 lbs, so they’re easy to pick up and move from one process to another. But they’re no lightweights when it comes to heavy-duty processes like welding. In fact, there’s already a range of cobot welding systems to choose from. Surprised? Don’t be. It’s just one more smart application for these flexible, cost-effective, and easy-to-program automation tools.
The flexibility and ease-of-programming of cobot-based welding systems make them especially well-suited for low-volume/high-mix environments, as well as custom or small-template welding processes. But with high accuracy and repeatability, these systems can also handle long runs with consistent quality. Welding tasks can be programmed in as little as half-an-hour by workers who have no previous experience, and programs can be saved and reused, saving the expense of trained robot programmers. Lightweight cobot welders can be mounted on tabletops, hung from ceilings, or installed into existing welding booths, offering more flexibility than manual welders or traditional fixed robots. And speaking of manual welders, these will be increasingly harder to find. In the U.S. alone, the American Welding Society predicts a shortfall of 372,000 welders by 2026.
Several companies have already announced cobot welding systems.

SNAPWELD SYSTEM CAN BE EASILY PROGRAMMED DIRECTLY THROUGH ROBOT’S TEACH PENDANT

SnapWeld system can be easily programmed directly through robot’s teach pendant
Universal Robots and ARC Specialties recently announced the first collaborative MIG welding system in the US at FABTECH 2017 taking place this week in Chicago. The SnapWeld Collaborative Robot Welding package is a cobot-assisted, interactive welding system that can be deployed in existing, manual welding booths, so it eliminates the need for costly new robotic cells. The system is ideal for small job shops that are struggling with the budget, programming, and space requirements of traditional welding robots

We are getting a lot of requests for integrating Universal Robots in welding booths, so we saw this as a unique opportunity to develop an integrated low-cost system for gas metal arc welding (GMAW) applications that no one else in the market is currently offering.

John Martin, Vice President of ARC Specialties

The SnapWeld system includes a Profax wire feeder and water-cooled torch for welds up to 600 amps, along with the UR robot. One of the big advantages of using cobots for a welding application is the ease of programming. SnapWeld was developed with and verified by Universal Robots through the UR+ platform facilitating direct software integration into the UR programming environment, enabling advanced settings to be easily programmed directly on the robot’s teach pendant.

Migatronic CoWelder is small and flexible enough to set up on a table in any shop

Another cobot welding system, the CoWelder, is available from Migatronic in Denmark. The CoWelder system includes a UR5 or UR10 robot—depending on payload and reach requirements—along with a Migatronic power source, start/stop safety box, and Migatronic welding torch and torch holder.

The system fits on a tabletop, making it ideal for even the smallest shops, with simple set-up and programming for significant savings over traditional complex robotic systems. The robotic welder ensures uniformity in series production, but it is so fast and easy to reprogram that it provides value even for small batches. For high-mix situations, shops can build a library of programs for different workpieces and easily switch among them during a workday.

Once the path is taught, SnapWeld will move along the start and stop path and weld only during specified stitch areas.SnapWeld attracted significant attendee and media attention at FABTECH where people often stood three rows deep to watch how easy it is to simply grab the robot arm and teach the welding path. The CoWelder at Danish manufacturer of animal housing, Jyden Bur A/S.Certified by Universal Robots.

Migatronic customer Sebastian Jacobsen, Project Manager at Jyden Bur A/S, Denmark says, “We can program new workpieces in no time. It really only takes 30 minutes for us to program a new workpiece and a few seconds to recall already stored programs. I don’t think it can get any easier.”
Speaking to productivity gains, Jens Christian Lægsgaard, General Manager of MVI Maskinfabrik in Denmark says, “Our time saved per workpiece is about 50%. We produce from ten to 1000 workpieces at a time. Our efficiency gains are 30-40% owing to the easy switching between programs and welded workpieces. And this is just the beginning…”

Cobots take on the welding world
As integrators look to provide high-ROI automation solutions, welding is a clear target. And integrators around the world are looking first to UR for the cobots to power their collaborative welding systems. Additional solutions have been announced from the Dutch integrator Cobot Automation and US-based SCOTT Automation (parent company of RobotWorx)

Think you are too small for robotics? Our short free ebook will guide you through the most important considerations for robotics in small and mid-sized manufacturing.

Avatar

Universal Robots

Universal Robots delivers industrial-grade collaborative automation built to perform, scale, and last. Combining lightweight, high-performance hardware with intuitive PolyScope software, certified safety, cybersecurity and open interfaces, Universal Robots enables manufacturers and integrators to deploy automation faster, reduce risk, and evolve toward AI-supported production—across applications, sites, and industries.

Automate with Confidence.