Only people can do that - creative people that problem-solve and improve products. A skilled cabinetmaker might see a piece of wood and say, 'this piece of wood would make a really fine table.' A robot cannot do that.
As of now, a big gap has materialized in the value-creation process after the first four industrial revolutions: Mechanization, electrification, automation, and now digitalization. It is this loss of value that the fifth industrial revolution should remedy.
The values in the world have been created through industrial production but the production environment has scared creative people away from the manufacturing industry. Now the new generation of collaborative robots enables us to view robots in a new way.
At the electronics manufacturer Wistron, they have embraced the opportunities in the new collaborative robot types, also called cobots, whole-heartedly. At Wistron robots and people work side-by-side interacting with one another, resulting in increased productivity, improved staff retention and, reduced training costs, and overall a much improved competitive edge.
The same happens on the BMW assembly line. The big breakthrough is the modern robot’s 'senses' in the form of sensors, cameras, and other safety features. Human intelligence works in tandem with robots, it’s a quantum leap from the conventional and potentially dangerous industrial robots.
Universal Robots create cobots, and cobots are realizing - to put it bluntly - the fifth industrial revolution. People can use cobots to build passion and soul into their products. Right in the factory where products are made.
Consumers are increasingly willing to pay a high price for specialized products because they want to feel special. An added bonus is that the manufacturer can increase the profit margin even though it costs extra to build more soul into these products.
So let’s get the robots out of the cages. The creative people into the manufacturing industry. And the soul back into the products.
At Universal Robots we're always looking for the talented, passionate people that will help us do just that. Check out our opportunities here.