Skip to main content

Robots play a hand in reshoring initiatives - UR cobots

The trend to outsource manufacturing operations to emerging markets for cost savings has taken a dramatic turn. With rapidly rising labor costs in countries such as China, manufacturers are seeing erosion in the cost advantages of manufacturing overseas. When combined with the complex logistics and added shipping times of...

Robots play a hand in reshoring initiatives - UR cobots
Robots play a hand in reshoring initiatives - UR cobots

The trend to outsource manufacturing operations to emerging markets for cost savings has taken a dramatic turn. With rapidly rising labor costs in countries such as China, manufacturers are seeing erosion in the cost advantages of manufacturing overseas. When combined with the complex logistics and added shipping times of offshoring, this has left manufacturers looking for new ways to save costs and increase productivity.

Automation using cost-effective, advanced robotics technologies is helping this shift by enabling companies of all sizes to remain cost-competitive while keeping their manufacturing operations at home.

In a recent report from Boston Consulting Group, BCG senior partner and research coauthor Harold L. Sirkin, stated, "The share of executives saying that their companies are actively reshoring production increased by 9% since 2014 and by about 250% since 2012. This suggests that companies that were considering reshoring in the past three years are now taking action.”

In the BCG survey, 56% of respondents believe that decreasing costs of automation have improved their product competitiveness, and 71% believe that advanced manufacturing technologies will improve the economics of localized production. Nearly three-quarters (72%) said they will invest in additional automation or advanced manufacturing technologies in the next five years.

Interestingly, this increase in automation is not expected to have a negative impact on employment. The report shows that 50% of respondents anticipate net manufacturing job creation during the next five years, with 74% citing access to the skilled workforce as a strong factor for moving production to the U.S.

RSS Manufacturing & Phylrich, a faucet-maker in Costa Mesa, CA, is a case in point. CEO Geoff Escalette stated that “The whole premise for our company is to bring manufacturing back to this country. Our new robot fits perfectly within that master plan.”

The company deployed a UR5 from Universal Robots as a cost-effective automation solution that could be easily moved between CNC machines, assembly lines, and tube benders. Escalette found the industrial robot arm from Universal Robots as he was researching ways to meet a new monthly order to produce 700 valves. He explains, “Our CNC machine can normally do 400 valves per month with two shifts, so we would have been forced to buy another machine even if we put a third shift on. With the higher run-rate using the UR5, none of this was necessary.”

The UR5 from Universal Robots provides improved flexibility and increased productivity, with an ROI within a few months. And its advanced safety features mean there are no additional costs for safety guarding.

Escalette readily admits his employees did not greet the UR5 with overwhelming enthusiasm when it first arrived. “They thought they were looking at their replacement. But now, we can educate and promote our employees from machine operators to robot programmers and quality control inspectors… When they realized how easy it was to use the Universal Robot and what they’ll eventually be doing with it, they all embraced it. Now they are excited to become the first guy that gets to start programming the robot.”

Avatar

Universal Robots

Universal Robots delivers industrial-grade collaborative automation built to perform, scale, and last. Combining lightweight, high-performance hardware with intuitive PolyScope software, certified safety, cybersecurity and open interfaces, Universal Robots enables manufacturers and integrators to deploy automation faster, reduce risk, and evolve toward AI-supported production—across applications, sites, and industries.

Automate with Confidence.