One tool with many applications
Cobots are a flexible and versatile automation solution. Compared to traditional industrial robots, they are quicker to install, simpler to operate, and suited for automating a wide range of processes commonly found in industrial and manufacturing environments.
Here are a few examples:
Case erecting and packing
Singapore-based Clearpack is a leading provider of packaging automation solutions in Southeast Asia, China, India, Middle East and Africa. It has created a compact palletizing solution that uses a UR10 cobot along with the LIFT KIT by Ewellix. The solution has helped multiple Clearpack customers optimize their warehouse space and remove the need for human workers to spend hours lifting heavy payloads.
It’s a case erecting and packing solution that works in a huge variety of industrial and manufacturing environments. It doesn’t take up much space, can be moved quickly around the production area using castor wheels, and the open platform means customers can modify it themselves after minimal training.
Get more information here.
Picking items from a moving conveyor belt
Norwegian meat producer Nortura didn’t have the space for a traditional industrial robot and the safety cages required to operate it safely. Using a UR10, an IFM 02D222 vision camera and a vacuum gripper, the company is able to achieve the same results with about 20% of the space requirements.
The system automatically detects when a pallet has been placed in front of it and then begins picking boxes off a moving conveyor belt and palletizing on its own. It is also able to vary the packing pattern for different products. One robot can process around 1,700 boxes, or 20 pallets, a day.
Read more about our work with Nortura here.