--

Cobots increase production volume by 20% while reducing customer rejections

Craft and Technik Industries

In short

After automotive component manufacturer Craft and Technik Industries (CATI) deployed collaborative robots for automatic inspection and CNC machine tending, efficiency has increased with production volume going up 15–20% with no defects or customer rejections.

Being an SME, most manufacturing tasks at CATI were handled manually but the company was facing problems finding manual labor, and was also looking for a way to reduce the number of customer rejections for faulty components.

Craft and Technik Industries

Industry Automotive and Subcontractors
Country Asia
Number of Employees 50-100
Cobots used UR10
Video — UR10 robots, Craft and Technik Industries (CATI), Pune, India

The solution

The key reason for implementing UR cobots was their collaborative safety features. At CATI, a lot of operators work on the shop floor and the company did not want to seclude an area because of the robotic operations.

The payload of the cobots was also imperative – the weight of the components manufactured by CATI range from about 1 – 5 kgs. Universal Robots’ largest model, the UR 10, lifts up to 10kgs, making for the perfect tool for CATI’s requirements.

The primary use of the UR10 is loading and unloading a vertical CNC machine. Additionally, the cobot is used for automatic inspection. Here, the cobot places a component on a weighing machine, takes feedback via digital input to decide whether the part meets its weight requirement or not, and then proceeds to sort the component accordingly.

Thus, customers are ensured that they do not receive any faulty components. The cobots, so far, have helped manufacture 40,000 parts, with zero defects or customer rejections.

By the time the cobot finishes weighing components from one machine, the second machine is ready with fresh components for the cobot to inspect, making for perfectly timed operations. CATI has already witnessed a 15-20% increase in its production after deploying the UR10, and is aiming for a 30% increase.

I have been to Japan and seen robots work on the assembly line at the same time as workers, but the problem is that the entire assembly line is fenced. Collaborative robots need no fencing and can easily work on the shop floor with my workforce. Since the deployment of cobots, all the parts manufactured and inspected have been perfect, with no customer rejections

EESHAN PRASHANT UMBRANI, COO, Craft and Technik Institutes (CATI)
Human and Robot working together

Human and Robot working together

“We talk about unemployment all over the country but the truth with the SME sector is that we actually can’t find enough qualified labor,” said Prashant Shantaram Umbrani, CEO of CATI. So, the best combination for us is incorporating robots in our manufacturing, alongside human workers. Smartly combining the number of machines and robots ensures that the payback period will be faster,” said the CEO, recommending his SME fraternity embrace automation. “The time has come for SMEs to automate – robots are no longer the prerogative of large-scale industries only.”

The product

The product

Established in 1996, Craft and Technik Industries (CATI) are manufacturers of precision components, mainly for the automobile industry. Their product range includes various pulleys, impellers, and gear and pump covers. As of 2018, they export 70% of their products. The deployment of UR cobots is a testament to CATI’s vision to explore automation and keep in line with the latest technology.

Easy-to-use

Easy-to-use

Easy-to-use UR cobots, even with no programming experience at Craft and Technik Industries (CATI), India

UR10 cobot

UR10 cobot

CNC machine tending and quality inspection applications by UR10 collaborative robot at Craft and Technik Industries (CATI), India

Automation challenges solved

  • Solves issue of labor scarcity faced by Indian SMEs competing with MNCs for manpower
  • Works in constrained area on shop floor
  • Increase in quality and quantity of output
  • Zero rejections ensured
  • Cobot(s) Deployed: 1 UR10

Key value drivers

  • Operates in constrained space without any cage
  • Collaborative and safe around employees
  • Perfectly timed operations
  • Ensures no defective parts reach customer

Tasks solved by collaborative robots

  • CNC
  • Machine Tending
  • Quality inspection

Get in touch with Universal Robots

Thousands of businesses rely on Collaborative Robots to...

  • Increase productivity
  • Adapt to changing product demand
  • Improve employee well-being and retention
  • Staff through labor shortages
Local Office
  • Universal Robots USA, Inc
  • 27175 Haggerty Road, Suite 160
  • 48377 Novi, MI
Contact us: +1 844-462-6268
Contact us: + 1-844-GO-COBOT