--

UR cobots improve productivity for plastic molding company

Linaset
Linaset

Linaset

UR5 cobot solution provides time and energy relief for plastic moulding manufacturer.

Universal Robots implemented its UR5 robotic arm solution for Linaset, helping to improve productivity and efficiency, while relieving staff members of a particularly time and energy consuming production line task.

Watch video

In short

Universal Robots implemented its UR5 robotic arm solution for Linaset, helping to improve productivity and efficiency, while relieving staff members of a particularly time and energy consuming production line task.

Supplying plastic mouldings to customers in the automotive and other industries, Linaset needed a safe, precise and efficient way to automate the component blasting stage of its process.

In the past, mouldings had been blasted manually on a worktable on both sides using a special blasting media – an operation that was both time and resource consuming when done completely manually.

As it was also necessary for the blast applicator to be held upright in a particularly dusty and noisy workplace, it was also a job that placed considerable physical demand on staff. All of this would need to be considered if a suitable automated solution was to be found.

Linaset

Industry Automotive and Subcontractors
Country Europe
Number of Employees 500-1000
Cobots used UR5
Video — UR5 robot, Linaset, Czech Republic

The solution

Linaset installed the UR5 robot arm and put it to work in test mode less than one week after ordering. Situated in the existing workplace and equipped with a simple fastener for attaching the blast media applicator, it worked together with human operators placing the mouldings into the jigs and rotating them during the cycle so the robot could blast both sides.

The immediate effect was the amount of time required for processing one moulding was reduced by as much as 30%, increasing productivity while ensuring premium levels of precision and quality. When the blasting media needed to be refilled, the robot would detect the low supply and stop automatically.

Over a six-month period, running continuously 24 hours a day and seven days a week, Linaset did not record a single malfunction or period of unplanned downtime for the UR5. And, aside from regular maintenance and cleaning dust from the control unit, there was no need to perform any service work or change parts – despite the harsh environment.

We were easily able to produce our own simple accessories for mounting the robot on the worktable and for attaching the blasting media applicator nozzle and we can also very easily program the robotic arm ourselves

Petr Šromota, Production Manager
Easy integration

Easy integration

According to Petr Šromota, major production manager at Linaset, the speed at which the robot became a flexible part of the manufacturing process was impressive. "There was no waiting time and within a few days, the robot was deployed at the workplace and began to operate reliably," he explains.

Automation for everyone

Automation for everyone

The UR5 was supplied by EXACTEC, who carried out the initial robot configuration and basic training, so employees could program and maintain the robot. Linaset now has a more productive process that is also more efficient - with consumption of blasting media reduced by 35%.

Automation challenges solved:

  • Performing repetitive and otherwise physically demanding tasks precisely on a mass scale.

Key value drivers:

  • Increased safety
  • Productivity and accuracy
  • Reduced costs
  • Fast return on investment

Tasks solved by collaborative robots

  • Injection moulding

Get in touch with Universal Robots

Thousands of businesses rely on Collaborative Robots to...

  • Increase productivity
  • Adapt to changing product demand
  • Improve employee well-being and retention
  • Staff through labor shortages
Local Office
  • Universal Robots USA, Inc
  • 27175 Haggerty Road, Suite 160
  • 48377 Novi, MI
Contact us: +1 844-462-6268
Contact us: + 1-844-GO-COBOT