Thousands of businesses rely on Collaborative Robots to...
- Increase productivity
- Adapt to changing product demand
- Improve employee well-being and retention
- Staff through labor shortages
Hearing aid manufacturer Oticon had been using robot technology for 10 years but as the minute components became increasingly smaller the existing two- and three-axes robots were no longer suitable. If for instance a small part got stuck in the mould the robotic arm could not perform the required lateral and vertical movements sufficiently to tip it out. Replacing their existing two- and three-axes robots with a six-axes UR5 allowed them to automate small production runs with many variables. Equally important, the dexterous robotic arm handles parts of only a millimeter in size with great precision.
Also, rapid advances in medical engineering have resulted in constantly changing production processes and a broader range of hearing aid models meant that new technology was required.
“The parts for modern hearing aids are getting smaller and are often only a millimetre in size. We looked for a solution that can suction small parts out of a mould. This was impossible manually. We needed a more flexible solution that would also be economically viable for smaller production runs”, says Arne Oddershede, group leader of the maintenance unit at Oticon.
Arne Oddershede, Group leader of the maintenance unitSince we produce different batch sizes and components when developing new products, it must be possible to easily reprogram the robot. With a traditional robot, this involves a computer and requires specially-trained staff. But with the UR5, any member of the technical staff can literally grab the robot and show it the motion sequence using waypoints
Oticon was convinced by the intuitive user guide and the precision of the UR5 robots. Mounted firmly to the injection moulding machine, the robotic arm can position itself over the mould and suction up to four plastic elements simultaneously using a specially designed vacuum system. Without damaging the sensitive elements. Once the parts have been removed, the robot draws away and the moulding machine prepares for a new operation. All components from the same batch are subsequently collected in separate tubes to ensure they can be traced correctly.
Because of its six axes the UR5 is very maneuverable and able to rotate or tilt the parts in order to lift them quickly out of the mould. The robot works in four- to seven-second cycles depending on the size of the production run and the component. The flexible deployment was another key value driver for Oticon.
Thousands of businesses rely on Collaborative Robots to...