--

UR cobots simplify production process and increase product quality

Ronet

In short

RONET SP. Has set up a fully automated production line based on a UR robot. The system combines picking and placing tasks with quality control, providing a complete, end-to-end solution that requires no human interaction.

With over 1000 different types of springs produced each year, Ronet was looking for a way to simplify the production process while increasing the overall quality of the product. The high quality standard was essential, as roughly 15 percent of the production output is exported. Returns on this product would not only damage the brand, it would be costly and time consuming. The robot also had to be able to work in close quarters with the current employees – preferably with little or no safety guarding.

Ronet

Industry Metal and Machining
Country Europe
Number of Employees 25-50
Cobots used UR5
UR5 collaborative robot, Ronet, PolandUR5 collaborative robot, Ronet, Poland

For our production line we have selected the robot from Universal Robots due to its unique features – among others versatility and the fact that the robot can work right alongside employees with no special safety guarding

Bogumił Zach, CEO

Fully automated production line

Ronet chose to work with Pol-Sver, the Polish UR distributor, to create a fully automated production line based on the UR5. The UR5 robot has payload capacity of 5 kg and an operating range of 850 mm. Thanks to its mobility and small dimensions it can also be used at other workstations in the production facility. The robot’s programming is very intuitive; an important criteria for the finished solution.

“We are betting on innovative manufacturing to guarantee highest quality of our products and improve the efficiency of the manufacturing process. For our production line we have selected the robot from Universal Robots due to its unique features – among others versatility and the fact that the robot can work right alongside employees with no special safety guarding” said Bogumił Zach, CEO of Ronet.

“For us intuitive operation and ease of programming were very important. The robot’s movement trajectory may be defined not only by using the control panel, but also by manually guiding the robot to the required position”. Ronet’s future plans call for even more robots, including construction of a fully automated manufacturing facility.

UR5 collaborative robot, Ronet, Poland
UR5 collaborative robot, Ronet, Poland

Automation challenges solved:

  • Relieved employees of strenuous, repetitive tasks.
  • Improved the overall quality of the product.

Key value drivers:

  • Easy programming
  • Flexible deployment
  • Collaborative and safe
  • Fast payback

Tasks solved by collaborative robots:

  • Pick and place
  • Quality inspection
  • Machine tending

Get in touch with Universal Robots

Thousands of businesses rely on Collaborative Robots to...

  • Increase productivity
  • Adapt to changing product demand
  • Improve employee well-being and retention
  • Staff through labor shortages
Local Office
  • Universal Robots USA, Inc
  • 27175 Haggerty Road, Suite 160
  • 48377 Novi, MI
Contact us: +1 844-462-6268
Contact us: + 1-844-GO-COBOT