<link rel="stylesheet" href="styles-3S7W63VL.css"> Skip to main content

Assembly line operations at Dutch automobile manufacturer

Automation at Stellantis

Video — Stellantis, Italy

In short

Stellantis N.V. is a Dutch multinational automobile manufacturer established through a merger between the PSA and Fiat Chrysler Automobiles groups. Stellantis has installed 11 Universal Robots collaborative robots at its Mirafiori factory in Turin, Italy, to automate a series of complex assembly line operations and quality controls for the new FIAT 500 electric car. The collaborative applications developed at Mirafiori have delivered significant benefits in terms of operating precision and quality, and also improved the ergonomics of a series of operations previously performed manually.

On the FIAT 500 electric car production line, some of the assembly processes and quality controls required the introduction of specific automation technologies to ensure the quality and repeatability needed to meet product standards. Additionally, given the fairly high average age of the factory workers, the question of ergonomic well-being was a keenly felt issue.

Stellantis decided to adopt Universal Robots collaborative robots some years ago. For the company UR technology has been a guarantee of a particularly advanced man-machine interface perfectly matched with the group's quality requirements in terms of both production processes and products. Collaborative automation has freed operators from repetitive and physically demanding manual tasks, so that they can be employed on processes with greater added value.

The 11 UR cobots now automate the following applications:

  • Application of the waterproof liner to the vehicle doors (2 UR10e cobots working in parallel)

  • Positioning of the soft-top (activation of the primer track and visual inspection to ensure the correct extrusion of the adhesive band around the perimeter) (1 UR10e)

  • Check on soft-top frame dimensions (1 UR10e)

  • Riveting of the tailgate with blind rivets press-set on the boot frame (1 UR10e)

  • Hood mounting (1 UR10)

  • Tightening of the rear side-door hinges (1 UR10)

  • Mudguard mounting (2 UR5 and 2 UR10 cobots)

Stellantis

Industry Automotive and Subcontractors
Country Europe
Number of Employees 1000+
Cobot used UR5 and UR10e

How they did it

How the FIAT 500 Assembly was optimized with Universal Robots collaborative robots

Introducing automation

Introducing automation

The Universal Robots collaborative robots at the Mirafiori factory were rolled out gradually to enable the operators to fully understand how the automated processes worked. “As a first step, we decided to introduce a UR cobot in the company canteen, distributing glasses of water to employees during the lunch break,” explains Mirafiori plant manager Luigi Barbieri. “This gave the line workers the opportunity to see the safety and collaborative nature of the cobots for themselves, and overcome any apprehensions about the safety of the subsequent applications.” After the success of this initial trial, the UR cobots were installed on a series of applications on the 500 electric car production line.

Cobot accuracy optimizes door assembly

Cobot accuracy optimizes door assembly

Two UR10e cobots operate in parallel on the door assembly line. A vision system registers the arrival of the door and activates the cobot, which uses a roller attached to its wrist to apply constant pressure on the fabric, applying it on the door panel. The application is particularly challenging because it requires the cobot to follow a complex path within a confined space, avoiding the panel's push pin protrusions and ensuring that the liner is completely sealed to prevent the infiltration of water. The cobots work with millimetric precision, guaranteeing a repeatability of +/- 0.05 mm.

On the FIAT assembly line

On the FIAT assembly line

Two UR10e cobots operate on the soft-top assembly line for the FIAT cabrio 500 model. The first cobot performs two different operations; Using a pad supported by a special pick-up device, the UR10e cleans and prepares the primer track, on which the adhesive to fix the soft-top to the frame is subsequently applied. The second operation is a quality control, where a vision system checks the geometric continuity and dimensions of the adhesive band.

Productivity and quality advantages

Productivity and quality advantages

The second cobot works in synergy with an anthropomorphic robot. Once the soft-top has been assembled, it is opened on a special support and then picked up by the robot. At this point, the second UR cobot runs a size check (through a vision system) on the soft-top frame to ensure the conformity of the dimensions. Once conformity has been ascertained, the soft-top is removed from the line by the anthropomorphic robot. This application offers a series of productivity and quality advantages. The cobots ensure that the adhesive extrusion is correct and check the dimensions of the soft-top frame.

We decided to adopt Universal Robots collaborative robots some years ago. For us, UR technology is a guarantee of a particularly advanced man-machine interface perfectly matched with the group's quality requirements in terms of both production processes and products.

Ennio Meccia, Head of Manufacturing Chief Engineers - STELLANTIS

Ensuring consistency on the assembly line

On the door assembly line for the FIAT 500 electric cabrio car, a UR10e cobot has been configured to press-set 10 blind pop rivets, which secure the boot hinge reinforcements to the boot frame. The operator loads the tailgate frame and hinge reinforcements on to the workstation, then leaves the cobot to position and press-set the rivets. The application provides productivity and ergonomic benefits. At the same time, constant monitoring of the workstation input and output parameters ensures higher and consistent process quality.

For the hood mounting application, the car body reaches the workstation with the hood mounted in a closed position and the hinge screws inserted by the operators on the previous station. Once the hood geometry has been established, the cobot (a UR10) moves into position and tightens the 4 screws to the correct torque. The main advantages of this application are quality, efficiency and ergonomics, given that the hood reaches the station in a closed position, making correct tightening extremely difficult. Since the hinge screws to be tightened are not visible, the operator could easily miss one or make an incorrect tightening. The cobot also improves the ergonomics of the operation, freeing the operators from working in uncomfortable or awkward positions.

Door hinge tightening and mounting

For the FIAT 500 model featuring an extra rear side door, an automated application capable of performing a complex tightening cycle was required. With the assistance of an advanced automated tool on which the cobot is installed, the door is positioned correctly on the vehicle body. The cobot then performs the tightening operations, from the rear of the boot. The cobot meets two different process requirements: it frees the operator from tightening the hinges in an awkward posture, where they would be unable to see the correct positions inside the car body; and it prevents the kickback from the tightening tool (which operates with a 75 Nm torque) hitting the arm of the operator.

In this station on the sheet metal line, the frame arrives with the right and left mudguards already in position. Two UR5 and two UR10s cobots are installed on a platform that lowers itself on the z axis in relation to the body. The wings of the platform close to fix the geometry and activate the tightening operation on the 24 screws that fasten the mudguards. Each of the 4 cobots is fitted with an automatic screw gun with torque control.

The application offers various advantages. Collaborative automation guarantees ergonomic benefits for the operators (who are no longer required to work below the vehicle body). Since the screws are torque tightened, tensile stress on the sheet metal parts is eliminated. Also, the cycle time is shortened, boosting the productivity of the whole station.

UR10e executes two different operations: cleans and prepares the primer track, on which the adhesive to fix the soft-top to the frame is subsequently applied, and executes is a quality control, where a vision system checks the geometric continuity and dimensions of the adhesive.The main benefit of the hood mounting application are quality, efficiency and ergonomics, given that the hood reaches the station in a closed position, making correct tightening extremely difficult for the operator.

Automation challenges solved:

  • Guaranteed ergonomics for complex assembly tasks
  • Guaranteed quality and repeatability on screw tightening
  • Checking of adhesive dispensing cycles and of assembly size conformity

Key value drivers:

  • Accuracy
  • Precision
  • Ergonomics

Tasks solved by collaborative robots:

  • Assembly, screw tightening, quality control, visual inspection, dispensing

Get in touch with Universal Robots

Thousands of businesses rely on Collaborative Robots to...

  • Increase productivity
  • Adapt to changing product demand
  • Improve employee well-being and retention
  • Staff through labor shortages