For Tomenson, collaborative automation was by far the best option, offering a small footprint, easy implementation, and safe operation around human workers. “The collaborative aspect of the robot system was absolutely necessary,” explains Roake. “We knew we were not going to get a gripper and robot that might need guarding because we’re working in a tight environment in the cell where they’re working. The collaborative aspect was one of the main factors in how we picked out the system.”
Tomenson chose to deploy a UR3 collaborative robot fitted with OnRobot’s RG6 gripper, driven by the complete solution's ease of use, small form factor and built-in safety features. The RG6 gripper is part of the UR+ platform, which means it’s certified to work seamlessly with UR cobots as the gripper’s control software comes fully integrated on the cobot’s teach pendant.
UR+ Products Used:
RG6 gripper from OnRobot