Hirebotics’ automation experts will visit your facility to work closely with the operations team. Together they will examine your process and determine where automation will have the strongest impact to make your factory more competitive on the world stage. Hirebotics will then design a comprehensive automation solution featuring state of the art robots from Universal Robots that will be installed and monitored 24 hours a day, providing you with access to all of the production data. All with no upfront costs to you. You simply pay for the robot as if it were another employee. Since you are only charged for the hours that the robots are productive, Hirebotics share the same goals. The more work Hirebotics can help you complete, the better off both companies are.
Hirebotics uses Universal Robots in the design and implementation of the robotic workers because of their inherent safety and the ability to set the robots up to work in close proximity to your human workers. By utilizing the advanced collaborative features of the robot they are able to achieve more by having humans and robots collaborate with each other. Studies have shown that human/robot collaboration generally yields higher productivity than either can reach alone. The reason for this is simple, you get the best of both worlds when you allow the robots and the humans do what they excel at. While humans are great at cognitive tasks or tasks that require dexterity or vision, robots excel at monotonous tasks, repetitive tasks, high precision tasks. By using both together, your human workers will have higher job satisfaction, and let’s face it, the robot never gets bored.
Expanding the workday, robot workers can often be designed to complete tasks while unattended at night, gaining additional hours of productive work every single day. Explore a world of real-time insight into how well your factory is operating. The mobile app dashboards give you access to data when you want it. See what is happening on your factory floor right now instead of seeing today’s production reports tomorrow. The system can alert you to prevent a potential problem from becoming a real problem. If the planned hourly production is 200 parts per hour, set a trigger to alert you if the rate drops. The system operates in real-time, alerting you, and allowing you to make corrections. You can even have your robots talk to you through the app, are their events that occur that you want to know about such as being without work for a specified time limit, or when there is a quality issue with the parts.