Collaborative robots (“cobots”) are being adopted at unprecedented rates, due in large part to their user-friendly design. This positive user experience is no fluke. It comes as a result of in-depth research and design and ongoing testing to explore how the robots are actually being used and how they can be continuously improved.
UX DESIGNER CONNECTS R&D TO THE REAL WORLD
Maren Nelson Hadar is a user experience (UX) designer with Universal Robots (UR) whose job is to connect the company’s R&D work with what’s happening in the field so that new products and features meet users’ needs. Hadar visits UR customers to see first-hand how they interact with the robots. “It’s not enough to just hear about what they’re doing,” explains Hadar. “You need to watch people and the robots in action to understand what problems they face on a daily basis.”
Hadar tries to meet with several typical robot users on her site visits, including the production manager, robot operator, and programmer. “The most interesting thing about visiting these companies is how different they are and how differently they use our robots,” says Hadar. “When I go to a smaller company, for instance, the person who programs the robot is often the same person who operates it, so it’s important that programming is easy to access and use. Larger companies might have those people in separate roles. In that case, the programmer might want to lock down the program so that operators just need to be able to start and stop the robot.”
THE USER’S JOURNEY STARTS BY UNBOXING THE ROBOT
Even though UR
cobots are easy to use, they’re still sophisticated robots. Some users are novice programmers or operators who aren’t aware of all of the robot’s functionality. UR is always looking at ways to improve the entire user journey, from unboxing to programming, addressing different levels of expertise. While Hadar is onsite, she may be able to point out what users can do to address a particular situation. At other times, the challenges users face provide feedback for where UR can improve, such as with new training material, manual content, and help features. By teaching people how to use the robots in the right way and to their fullest capacity, that can circumvent many challenges that users might experience.
Hadar’s research could ultimately lead to changes in the graphical user interface (GUI) used to program the robots, or where connectors should be located on the robot itself—anything that can improve the user experience. “It’s interesting to see so many different contexts where the robots are being used, but that also makes it very challenging for us,” Hadar explains. “We have to understand all these different interactions, which means that different users will have a very different sense of satisfaction. We need to meet all those needs.”