COBOTS IN THE INDUSTRY.
There are many reasons to implement a
collaborative robot or “
cobot” from Universal Robots. Manufacturers love their flexibility and ease-of-use, and that they provide the fastest payback in the industry at only 195 days. But cobots from Universal Robots continue to bring significant value for years to come—long after that initial payback period.
A survey of our users reveals that despite being put through heavy-duty cycles year after year, the cobots are still running strong, in applications that include pick-and-place, gluing, welding, and assembly, and machine-tending.
Paul Quitzau, senior engineering manager at medical device manufacturer Tegra Medical
“We just achieved the one-millionth part out of our UR5 cell in less than a year. The accuracy and repeatability overtime was a big concern for us. We were apprehensive, questioning whether we could put the robot through this kind of duty cycle in a high-volume cell and get year-after-year repeatability. We spot-check the robot every few months to make sure the axes are performing and it is as good today as a year ago when we turned the cell on.
“Our team likes knowing that spare parts are held at their distributor’s facility or at a local UR office that can overnight parts if need be. We didn’t have such a great experience with some of our other robotic applications. If a robot went down, it was time trouble-shooting over the phone. It was a week or two of downtime waiting to get parts in, followed by an external engineer having to come in and install and requalify it. With the UR robot’s modular design, we can install parts ourselves without being handcuffed to an integrator. We think this is a better way to go for high-volume cells.”
Lars Bak, plant manager at gear manufacturer BJ Gear
“Six years after we bought our first robot, it is still in operation 14 hours a day, feeding pieces into a lathe, a cutter, and a washing machine. The robot has had two joint replacements over the years, but we keep extra joints in stock and can easily exchange the joint by ourselves. Our UR5 has proven to be an incredibly stable robot. We have not experienced any downtime with it despite putting it through high duty cycles for so many years.
“After having successfully installed the machine-tending application, we bought another UR5 five years ago to automate the spray painting of gear wheels. The robot is used even on small series down to five workpieces each. It is in continuous operation 6 hours a day, spray painting an ever-expanding array of gear wheels. We have had one joint replacement on it in five years. I’m very happy with the longevity of these robots.”