Scan time for CB3 and e-Series controller I/O
The listed scan times for inputs is the maximal time delay it takes from a signal has changed on the input pin to the change is registered by the controller.
The listed scan times for outputs is the maximal time delay it takes from a signal is set in the program execution of the controller to the output pin reads the same value.
The scan times for CB3 are
Summary of digital in- and outputs:
Summary of tool digital in- and outputs:
|
24 ms |
Timing demands for Safety outputs. Maximum accepted delay between first and second channel. |
Output: 8 ms |
Timing demands for Safety inputs.
|
CB3 Software BEFORE 3.2.18654: Inputs: 40 ms --------------------------------------------------- CB3 software AFTER 3.2.18654: Inputs: 40 ms 3-position enabling switch: 1000 ms |
The scan times for e-Series are
Summary of digital in- and outputs: Summary of analog in- and outputs: Summary of configurable in- and outputs:
Summary of tool digital in- and outputs:
Summary of tool analog inputs: |
4 ms |
Safety inputs: *Configurable inputs used for safety: |
7 ms |
Timing demands for Safety outputs. Maximum accepted delay between first and second channel |
Output: 1ms Note: If this does not happen, the robot will fault after 48ms |
Timing demands for Safety inputs. Maximum accepted delay between first and second channel. This is controlled by the safety control board (SCB). |
Inputs:40 ms 3-position enabling switch: 1000 ms |