The GRIP Base Connector allows quick and easy removal of the entire robot arm. The Robot arm is bolted to a quick Connect system which in turn is bolted to a table or cell. This manual Connect system allows companies to use the same robot in multiple different cells without having to unscrew the robot every time. A simple lever allows the robot to be released from its current position and taken to a new position. The entire process takes only a few seconds. It enables companies to be more flexible with the robots that they have and optimizes the use of their resources. In case of extreme loads we recommend the Base Connector SWS200.