The Kenos® Sack Gripper (KSG) is a dedicated solution to handle hard and soft bags usually dropped by conventional foam grippers and suction cups. It can be configured as you wish. Changing not only the size of the cup but also the vacuum generation, internal or deported, or the performance of the foam between three types of rings.
This gripper can work as well with cement bags in a dusty environment as with wrapped food products on a packaging line.
The gripper comes with the fixture, the control valve, and the URCap plugin for seamless integration.