<link rel="stylesheet" href="styles-3S7W63VL.css"> Skip to main content
Adaptive Suction Hand

Adaptive Suction Hand

Adaptive suction hand has a structure in which 12 shafts follow the irregularities of the workpiece and lock at the same time to fix it in place. As a result, even workpieces with complex shapes can be stably picked up, and it is possible to transport and seat them while maintaining the posture at the time of pickup.Since it can handle multiple workpieces, it is possible to achieve standardization of hands, reduce setup changes, reduce hand storage space, and reduce costs.

Read more
Manufacturer:THK CO.,LTD

Overview

Adaptive suction hand has a structure in which 12 shafts follow the irregularities of the workpiece and lock at the same time to fix it in place. As a result, even workpieces with complex shapes can be stably picked up, and it is possible to transport and seat them while maintaining the posture at the time of pickup.Since it can handle multiple workpieces, it is possible to achieve standardization of hands, reduce setup changes, reduce hand storage space, and reduce costs.

This hand can be directly attached to the arm with the included bolts and operates with only one attached air supply tube, a relay cable that can be connected to the M8 connector at the tip of the arm. Easily control suction ON/OFF and shaft lock by operating URCap.

Contact us

Your inquiry will be sent to our partner, who will contact you as soon as possible.