Let's connect electrical equipment to the robot through the M8 tool connector.
The Tool Connector, located at the end of the robot arm on the tool flange, provides various interfaces for connecting end effectors and tooling. For e-Series, the adapter is male, while UR20 and UR30 are equipped with a female connector.
The Tool Connector will most often be used with a ready-made end effector from UR+ where power and communication will often be transferred in 1 cable. However, the tool connector interface can be adjusted to many different needs.