Welding is an outstanding and hard to master craft, but unfortunately, it is becoming an increasingly lost one. Manual welding requires a trained human eye and impressive dexterity for the most complex welds. However, automated welding tools are becoming critical in helping businesses beat the lack of skilled welders and meet demand.
Adding a welding tool such as a collaborative robot (cobot) to do the repetitive, heavy-lifting welds enables you to do more and produce more parts, while freeing your experienced welders to focus on more exciting and complex welds.
With a robotic welding tool, you can achieve greater precision, speed, and consistency in every weld. Cobots can handle MIG, TIG, cutting (both plasma and oxy-fuel) as well as laser, spot and orbital welding.
Our welding systems are flexible, quick to deploy, straightforward for your welders to program, and customizable to meet the specific needs of your business. There are many advantages of using a robotic welding tool at your shop, including:
GREG LEFEVRE CEO and President at Raymath, USAThe learning curve isn’t as steep as what people think it is. The cost to get into it isn’t as much as people think. Don’t be afraid to take that step. You’re going to find out that even if it doesn’t go perfect, that ROI is going to be there in a pretty short time.
From initial project idea to striking the first arc, Universal Robots provides you with expert advice and the resources to get your cobot welding system running quickly and efficiently.
Following a preliminary assessment of your project’s specific needs, UR will connect you with the partner best suited to deliver a low-risk, tailored welding solution for your business.
Let's help you find a solution that fits the resources available and technical skills within your company, and that can efficiently handle the boxes and patterns you need to stack.
Selecting the right cobot for your welding solution is a crucial first step to its success. UR10e and the UR20 cobots are the most recommended for welding due to their reach, payload capacity, and precision.
UR10e is a flexible cobot with a 12.5 kg payload capacity, widely used in welding solutions.
UR20 is a cobot built for heavier payloads (up to 20 kg), faster speeds, and superior motion control.
Keep exploring the benefits of automated welding and learn how businesses from different industries have been using collaborative robots to perform their welding tasks.