@ProviderType
public interface TCPConfiguration
With this interface, it it possible to add a TCP for a device to PolyScope as well as update the TCP's offset and remove the TCP again.
Note: Any attempts to overwrite (calling thesetTCP(String, Pose)
method when a TCP has already been
added), remove or update an existing TCP are ignored when an existing installation is loaded. This is to ensure that
the end user’s previous settings are retained and not unintentionally modified.Modifier and Type | Method and Description |
---|---|
TCP |
getTCP() |
void |
removeTCP()
Remove the TCP of the device.
|
void |
setTCP(String suggestedName,
Pose tcpPose)
Add a TCP for the device to PolyScope.
|
void |
updateTCP(Pose tcpPose)
Update the offset of the device's TCP.
|
void setTCP(String suggestedName, Pose tcpPose)
Add a TCP for the device to PolyScope.
There can only exist one TCP for the device. If a TCP has already been defined, it will be overwritten with the new TCP.suggestedName
- Suggested name for the TCP. Valid names must match regex [a-zA-Z][a-zA-Z0-9_]{0,14} for a
total of 15 characters. The final name can be retrieved from the TCP instance (see getTCP()
).tcpPose
- A pose for the offset of the TCP with respect to the tool output flangeIllegalTCPNameException
- If the suggested name does not match required regex.IllegalArgumentException
- If any of the values of the pose specified for the TCP offset are not inside the
valid range of a TCP offset as defined by PolyScope.void updateTCP(Pose tcpPose)
tcpPose
- The pose for the new offset to set for the TCP with respect to the tool output flange.void removeTCP()
TCP getTCP()
Copyright © 2024. All rights reserved.