public interface WaitNodeConfigFactory
Modifier and Type | Method and Description |
---|---|
AnalogInputCurrentWaitNodeConfig |
createAnalogInputCurrentConfig(AnalogIO input,
CompareOperator compareOperator,
Current current,
ErrorHandler<Current> errorHandler)
Creates a configuration for waiting for an analog input to go past an electric current threshold.
|
AnalogInputVoltageWaitNodeConfig |
createAnalogInputVoltageConfig(AnalogIO input,
CompareOperator compareOperator,
Voltage voltage,
ErrorHandler<Voltage> errorHandler)
Creates a configuration for waiting for an analog input to go past a voltage threshold.
|
DigitalInputWaitNodeConfig |
createDigitalInputConfig(BooleanRegister input,
boolean valueToWaitFor)
Creates a configuration for waiting for a boolean register to go
true or false . |
DigitalInputWaitNodeConfig |
createDigitalInputConfig(DigitalIO input,
boolean valueToWaitFor)
Creates a configuration for waiting for a digital input to go high or low.
|
DigitalInputWaitNodeConfig |
createDigitalInputConfig(ModbusIO input,
boolean valueToWaitFor)
Creates a configuration for waiting for a digital MODBUS input to go high or low.
|
ExpressionInputWaitNodeConfig |
createExpressionInputConfig(Expression expression)
Create a configuration for waiting for an expression to be evaluated to true.
|
FloatRegisterInputWaitNodeConfig |
createFloatRegisterInputConfig(FloatRegister input,
CompareOperator compareOperator,
float valueToWaitFor)
Creates a configuration for waiting for a register to go past a float threshold.
|
TimeWaitNodeConfig |
createTimeConfig(Time time,
ErrorHandler<Time> errorHandler)
Creates a configuration for waiting a specified amount of time.
|
TimeWaitNodeConfig createTimeConfig(Time time, ErrorHandler<Time> errorHandler)
time
- the time to wait, not null
.errorHandler
- handler for validation errors. If using ErrorHandler.AUTO_CORRECT
this will clamp the value to the nearest valid time value.DigitalInputWaitNodeConfig createDigitalInputConfig(DigitalIO input, boolean valueToWaitFor)
input
- the digital input on which to wait, not null
.valueToWaitFor
- true
, if waiting for the input signal value/level to go HIGH, false
otherwise (waiting for LOW signal value/level).IllegalArgumentException
- if input
is an output (does not support reading of values).
See IO.isInput()
.DigitalInputWaitNodeConfig createDigitalInputConfig(ModbusIO input, boolean valueToWaitFor)
input
- the digital MODBUS input on which to wait, not null
.valueToWaitFor
- true
, if waiting for the input signal value/level to go HIGH, false
otherwise (waiting for LOW signal value/level).IllegalArgumentException
- if input
is an output (does not support reading of values)
or if output
is not a digital output. See IO.isInput()
and IO.getType()
.DigitalInputWaitNodeConfig createDigitalInputConfig(BooleanRegister input, boolean valueToWaitFor)
true
or false
.input
- the boolean register input on which to wait, not null
.valueToWaitFor
- true
, if waiting for the register to be true
, false
otherwise.IllegalArgumentException
- if input
is an output (does not support reading of values). See IO.isInput()
.AnalogInputCurrentWaitNodeConfig createAnalogInputCurrentConfig(AnalogIO input, CompareOperator compareOperator, Current current, ErrorHandler<Current> errorHandler)
input
- on which to wait, not null
.compareOperator
- the operator to use when comparing input to value, not null
. Available options are
"less than" (<) or "greater than" (>).current
- the electric current threshold to wait for, not null
.errorHandler
- the error handler for validation errors. If using ErrorHandler.AUTO_CORRECT
this will clamp the value to the nearest valid current value.IllegalArgumentException
- if input
is an output (does not support reading of values). See IO.isInput()
.AnalogInputVoltageWaitNodeConfig createAnalogInputVoltageConfig(AnalogIO input, CompareOperator compareOperator, Voltage voltage, ErrorHandler<Voltage> errorHandler)
input
- on which to wait, not null
.compareOperator
- the operator to use when comparing input to value, not null
. Available options are
"less than" (<) or "greater than" (>).voltage
- the voltage threshold to wait for, not null
.errorHandler
- the error handler for validation errors. If using ErrorHandler.AUTO_CORRECT
this will clamp the value to the nearest valid voltage value.IllegalArgumentException
- if input
is an output (does not support reading of values). See IO.isInput()
.FloatRegisterInputWaitNodeConfig createFloatRegisterInputConfig(FloatRegister input, CompareOperator compareOperator, float valueToWaitFor)
input
- the float register input on which to wait, not null
.compareOperator
- the operator to use when comparing register to value, not null
. Available options
are "less than" (<) or "greater than" (>).valueToWaitFor
- the float threshold to wait for.IllegalArgumentException
- if input
is an output (does not support reading of values). See IO.isInput()
.ExpressionInputWaitNodeConfig createExpressionInputConfig(Expression expression)
expression
- the expression to evaluate, not null
.Copyright © 2024. All rights reserved.