public interface KeyboardInputFactory
Factory for creating keyboard inputs which are used to configure the virtual keyboard/keypad and to request it to be
displayed for a Swing GUI component. The typical Swing component most commonly used is a JTextField
.
SwingProgramNodeService
,
SwingInstallationNodeService
and
SwingToolbarService
).Modifier and Type | Method and Description |
---|---|
KeyboardNumberInput<Double> |
createDoubleKeypadInput()
Creates a virtual numeric keypad input accepting doubles
|
KeyboardNumberInput<Integer> |
createIntegerKeypadInput()
Creates a virtual numeric keypad input accepting integers.
|
KeyboardTextInput |
createIPAddressKeyboardInput()
Creates a virtual keyboard input accepting IPv4 addresses.
|
KeyboardTextInput |
createPasswordKeyboardInput()
Creates a standard virtual keyboard input accepting password string/text input.
|
KeyboardNumberInput<Double> |
createPositiveDoubleKeypadInput()
Creates a virtual numeric keypad input accepting positive doubles.
|
KeyboardNumberInput<Integer> |
createPositiveIntegerKeypadInput()
Creates a virtual numeric keypad input accepting positive integers.
|
KeyboardTextInput |
createStringKeyboardInput()
Creates a standard virtual keyboard input accepting string/text input
|
KeyboardTextInput createStringKeyboardInput()
Creates a standard virtual keyboard input accepting string/text input
If no input validator is specified, all strings are accepted.KeyboardTextInput createPasswordKeyboardInput()
Creates a standard virtual keyboard input accepting password string/text input. When the end user types, asterisks are shown instead of the original characters.
If no input validator is specified, all strings are accepted.KeyboardTextInput createIPAddressKeyboardInput()
KeyboardTextInput
.KeyboardNumberInput<Double> createDoubleKeypadInput()
Creates a virtual numeric keypad input accepting doubles
If no input validator is specified, all double values are accepted.KeyboardNumberInput<Double>
.KeyboardNumberInput<Double> createPositiveDoubleKeypadInput()
Creates a virtual numeric keypad input accepting positive doubles. The minus ('-') button on the keypad will be disabled.
If no input validator is specified, all positive double values are accepted.KeyboardNumberInput<Double>
.KeyboardNumberInput<Integer> createIntegerKeypadInput()
Creates a virtual numeric keypad input accepting integers. The dot ('.') button on the keypad will be disabled.
If no input validator is specified, all integer values are accepted.KeyboardNumberInput<Integer>
.KeyboardNumberInput<Integer> createPositiveIntegerKeypadInput()
Creates a virtual numeric keypad input accepting positive integers. The minus ('-') and the dot ('.') buttons on the keypad will be disabled.
If no input validator is specified, all positive integer values are accepted.KeyboardNumberInput<Integer>
.Copyright © 2024. All rights reserved.