Interface | Description |
---|---|
FeatureVariable |
A Feature marked as a Variable in the installation will exist even when a robot is turned off and on.
|
GlobalVariable |
Global variables are available everywhere in a program.
|
PersistedVariable |
This interface represents variables stored with the installation.
|
ValuePersistedVariable |
This interface represents variables stored with the installation.
|
Variable | |
VariableFactory |
This interface supplies methods to create variable objects.
|
VariableModel |
Provides methods that returns the variables that currently are registered in the system.
|
Class | Description |
---|---|
VariableFilterFactory |
This interface provides predefined filters that can be used when searching for particular types of variables.
|
Enum | Description |
---|---|
Variable.Type |
The variable type used to determine which type of variable this instance is.
|
Exception | Description |
---|---|
VariableException |
This exception is thrown if a Variable has an illegal name.
|
Copyright © 2024. All rights reserved.