public interface PersistedVariable extends GlobalVariable
Variable.Type
Modifier and Type | Method and Description |
---|---|
boolean |
isResolvable()
A persisted variable can not be guaranteed to be present.
|
boolean isResolvable()
A persisted variable can not be guaranteed to be present. This method can be used to determine, if the variable is present.
The persisted variable will not be present, if the end user loads a different installation which does not contain the variable, or if the variable is deleted by the end user.
A program node storing aPersistedVariable
instance in its Data Model will be undefined if the variable
cannot be resolved (i.e. the variable is not present).true
if this persisted variable is present in the PolyScope installation, otherwise false
.Copyright © 2024. All rights reserved.