Interface | Description |
---|---|
GripperList |
This is the unmodifiable list of individual grippers available in a multi-gripper device.
|
GripperListBuilder |
This interface is used for creating the list of individual grippers/zones available in a multi-gripper device, i.e.
|
GripperListProvider |
This interface must be implemented by the gripper URCap to register the multi-gripper capability.
|
RegisteredCapabilities |
Each of the individual grippers/zones available in a multi-gripper device supports all capabilities that has been
registered, i.e.
|
Exception | Description |
---|---|
DuplicateGripperID |
This exception is thrown when an attempt is made to add a new gripper/zone to the list of individual grippers/zones
with an identifier, which is already used by a previously added gripper/zone.
|
DuplicateGripperName |
This exception is thrown when an attempt is made to add a new gripper/zone to the list of individual grippers/zones
with a name, which is already used by a previously added gripper/zone.
|
LessThanTwoGrippers |
This exception is thrown by
GripperListBuilder.buildList() , if an attempt is made to build the list of
individual grippers/zones when less than two grippers/zones have been added. |
Copyright © 2025. All rights reserved.