@ProviderType
public interface GripperRegistrationConfiguration
This interface represents the registration of a conformant gripper device. It is returned when a program node
contribution is registered as a conformant gripper by calling GripperRegistrationManager.registerAsGripper(Class)
.
Through this interface, it is possible to register any additional capabilities supported by the gripper besides basic
simple grip and release actions, such as force gripping and support for multiple individual grippers. This will enable
other program node contributions (for example contributed by other 3rd party URCaps) to configure the parameters of
each of the registered capabilities when creating GripperNode
configurations for the corresponding program node
contribution (which is registered as a conformant PolyScope gripper device).
SwingProgramNodeService.configureContribution(ContributionConfiguration)
(for Swing-based URCaps) or
ProgramNodeServiceConfigurable.configureContribution(ProgramNodeConfiguration)
(for HTML-based URCaps).Modifier and Type | Method and Description |
---|---|
GripperCapabilities |
getGripperCapabilities()
Access an interface that can be used for registering various capabilities supported by the gripper, such as force
gripping and support for multiple individual grippers.
|
GripperCapabilities getGripperCapabilities()
Access an interface that can be used for registering various capabilities supported by the gripper, such as force gripping and support for multiple individual grippers.
Note: All capabilities must be registered once upfront, and these one-time registrations must all occur within the scope of the call to eitherSwingProgramNodeService.configureContribution(ContributionConfiguration)
(for Swing-based URCaps) or
ProgramNodeServiceConfigurable.configureContribution(ProgramNodeConfiguration)
(for HTML-based URCaps).Copyright © 2025. All rights reserved.