Package | Description |
---|---|
com.ur.urcap.api.contribution.driver.screwdriver |
Modifier and Type | Method and Description |
---|---|
void |
ScrewdriverContribution.configureInstallation(CustomUserInputConfiguration customConfiguration,
SystemConfiguration systemConfiguration,
TCPConfiguration tcpConfiguration,
ScrewdriverAPIProvider apiProvider)
When this method is called, required configuration related to the setup of the screwdriver can be defined/performed,
e.g.
|
void |
ScrewdriverContribution.configureScrewdriver(ScrewdriverConfiguration screwdriverConfiguration,
ScrewdriverAPIProvider apiProvider)
When this method is called, use the configuration parameter to register or setup optional properties and capabilities
of the screwdriver.
|
Copyright © 2025. All rights reserved.