Interface | Description |
---|---|
AnalogInputUntilNodeConfig | |
BlendParameters | |
CustomBlendParameters | |
CustomDecelerationParameters | |
DecelerationParameters | |
DigitalInputUntilNodeConfig | |
DistanceUntilNodeConfig | |
ExpressionUntilNodeConfig | |
FloatRegisterInputUntilNodeConfig | |
IOInputUntilNodeConfig | |
ReachedWaypointUntilNodeConfig | |
UntilNodeConfig |
This interface represents a configuration of the Until program node.
|
UntilNodeConfigFactory |
This interface can be used to create configurations that can be applied to an Until program node.
|
Enum | Description |
---|---|
AnalogInputUntilNodeConfig.InputDomainType |
The type of the electrical domain used by an analog input.
|
BlendParameters.ParameterType |
Blend Parameters can be of different types
The parameter type is used to determine the explicit blend parameters (can be used in place of instanceof operations).
|
CustomDecelerationParameters.Type | |
DecelerationParameters.ParameterType |
The deceleration parameter type used to determine which type of deceleration parameter this instance is.
|
IOInputUntilNodeConfig.SelectionType |
The type of the input selection.
|
UntilNodeConfig.ConfigType |
The configuration type used to determine which type of configuration this instance is.
|
Copyright © 2025. All rights reserved.