Interface | Description |
---|---|
BlendParameters | |
FixedPositionDefinedWaypointNodeConfig |
This interface represents a fixed position configuration for a Waypoint node which has a defined Cartesian location
(i.e.
|
FixedPositionWaypointNodeConfig | |
JointMotionParameters | |
TimeMotionParameters | |
ToolMotionParameters | |
VariablePositionDefinedWaypointNodeConfig | |
VariablePositionWaypointNodeConfig | |
WaypointBlendParameters | |
WaypointMotionParameters | |
WaypointNodeConfig | |
WaypointNodeConfigFactory |
Enum | Description |
---|---|
BlendParameters.ParameterType |
The blend parameters type used to determine which type of blend parameters this instance is.
|
FixedPositionWaypointNodeConfig.PositionDefinition | |
VariablePositionWaypointNodeConfig.VariableDefinition | |
WaypointMotionParameters.ParameterType | |
WaypointNodeConfig.ConfigType |
The configuration type used to determine which type of configuration this instance is.
|
Exception | Description |
---|---|
IncompatibleMotionParameters |
This exception is thrown when trying to set Motion Parameters on the Waypoint node that is incompatible with the
Movement Type of the parent Move node.
|
Copyright © 2025. All rights reserved.