Interface | Description |
---|---|
AnalogInputDomainConfig |
This interface represents the analog input domain configuration for the two analog inputs in the Tool I/O Interface.
|
AnalogInputModeConfig |
This interface represents a configuration of the analog inputs in the Tool I/O Interface.
|
CommunicationInterfaceConfig |
This interface represents the Tool Communication Interface (TCI) configuration for the two analog inputs in the Tool
I/O Interface.
|
DigitalOutputModeConfig |
This interface represents a configuration of the output mode for the digital outputs in the Tool I/O Interface.
|
StandardDigitalOutputModeConfig |
This interface represents the digital output mode configuration for the digital outputs in the Tool I/O Interface.
|
ToolIOInterface |
This interface allows for querying the settings of the Tool I/O Interface
|
Enum | Description |
---|---|
AnalogInputDomainConfig.AnalogDomain |
The type of the electrical domain used by the analog inputs in the connector in the robot tool
|
AnalogInputModeConfig.ConfigType |
The configuration type used to determine which type of configuration this instance is.
|
CommunicationInterfaceConfig.BaudRate |
Available options for the baud rate used for communication
|
CommunicationInterfaceConfig.Parity |
Available options for the parity used for communication
|
CommunicationInterfaceConfig.StopBits |
Available options for the number of stop bits used for communication
|
DigitalOutputModeConfig.ConfigType |
The configuration type used to determine which type of configuration this instance is.
|
StandardDigitalOutputModeConfig.OutputMode |
Available output modes for the digital outputs in the connector in the robot tool.
|
ToolIOInterface.OutputVoltage |
Available options for the output voltage level for the power supply that delivers power to the connector in the
robot tool
|
Copyright © 2025. All rights reserved.