@ProviderType
public interface RobotModel
Modifier and Type | Interface and Description |
---|---|
static class |
RobotModel.RobotSeries
Deprecated.
See
getRobotSeries() |
static class |
RobotModel.RobotType
The different types/models of Universal Robots robots
|
Modifier and Type | Method and Description |
---|---|
RobotLimits |
getRobotLimits()
Each Universal Robots robot type/model has limits for various physical/hardware and software properties/parameters.
|
RobotModel.RobotSeries |
getRobotSeries()
Deprecated.
This method can only be used to determine, if a robot belongs to the CB3 robot series. The method will
return the value
RobotModel.RobotSeries.CB3 , if the underlying robot is a CB3 robot, whereas the
RobotModel.RobotSeries.E_SERIES value is returned for an e-Series robot. The RobotModel.RobotSeries.UNKNOWN value will be
returned for all robots belonging to other robot series. |
RobotModel.RobotType |
getRobotType() |
String |
getSerialNumber() |
RobotModel.RobotType getRobotType()
@Deprecated RobotModel.RobotSeries getRobotSeries()
RobotModel.RobotSeries.CB3
, if the underlying robot is a CB3 robot, whereas the
RobotModel.RobotSeries.E_SERIES
value is returned for an e-Series robot. The RobotModel.RobotSeries.UNKNOWN
value will be
returned for all robots belonging to other robot series.RobotLimits getRobotLimits()
Each Universal Robots robot type/model has limits for various physical/hardware and software properties/parameters. This method can be used to obtain an interface which provides access to the valid range for each property/parameter supported by the underlying robot, such as the supported range for the mass of the payload attached to the robot's tool output flange.
These ranges (limits) can, for instance, be used for validation of input provided by the end user.String getSerialNumber()
Copyright © 2025. All rights reserved.