public static enum MomentOfInertia.Unit extends Enum<MomentOfInertia.Unit>
Enum Constant and Description |
---|
KG_M2
Kilograms * meters^2 [kg*m^2] SI unit.
|
LB_FT2
Pound * feet^2 [lb*ft^2] imperial unit.
|
Modifier and Type | Method and Description |
---|---|
static MomentOfInertia.Unit |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static MomentOfInertia.Unit[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final MomentOfInertia.Unit KG_M2
public static final MomentOfInertia.Unit LB_FT2
public static MomentOfInertia.Unit[] values()
for (MomentOfInertia.Unit c : MomentOfInertia.Unit.values()) System.out.println(c);
public static MomentOfInertia.Unit valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2025. All rights reserved.