AnalogInputUntilNodeConfig |
AnalogInputUntilNodeConfig.InputDomainType
The type of the electrical domain used by an analog input.
|
BlendParameters |
BlendParameters.ParameterType
Blend Parameters can be of different types
The parameter type is used to determine the explicit blend parameters (can be used in place of instanceof operations)
|
CustomDecelerationParameters |
CustomDecelerationParameters.Type |
DecelerationParameters |
DecelerationParameters.ParameterType
The deceleration parameter type used to determine which type of deceleration parameter this instance is.
|
DigitalInputUntilNodeConfig |
DistanceUntilNodeConfig |
ExpressionUntilNodeConfig |
FloatRegisterInputUntilNodeConfig |
IOInputUntilNodeConfig |
IOInputUntilNodeConfig.SelectionType
The type of the input selection
|
ReachedWaypointUntilNodeConfig |
UntilNodeConfig
This interface represents a configuration of the Until program node.
|
UntilNodeConfig.ConfigType
The configuration type used to determine which type of configuration this instance is.
|