public interface InstallationNodeService
Modifier and Type | Method and Description |
---|---|
InstallationNodeContribution |
createInstallationNode(URCapAPI api,
DataModel model)
Creates a new installation node instance.
|
InputStream |
getHTML() |
String |
getTitle() |
String getTitle()
InputStream getHTML()
InstallationNodeContribution createInstallationNode(URCapAPI api, DataModel model)
Creates a new installation node instance.
The returned node must use the supplied data model object to retrieve and store the data contained in it. All modifications to the supplied data model from the installation node constructor are ignored when an existing installation is loaded. The data model object is shared between all installation nodes contributed by the same URCap.api
- object with access to PolyScope functionality.model
- object where all configuration data of the new installation node.
instance is to be stored in and retrieved from.Copyright © 2023. All rights reserved.